D-sub connector: 5 ways to differentiate D-sub connectors

게시자

D-sub miniatures, also called D-sub connectors, are small electrical connectors that are commonly used in computer communication applications. Since their inception in 1952, manufacturers value D-sub connectors for their reliability and durability.

Whether you plan to utilize a D-sub connector in your device's network, video, or other communication ports, double-check all of your design parameters before you select a connector. Let's review five critical factors that differentiate D-subminiature connectors to help you streamline your next application.

1. D-sub connector gender

Like nearly all connector types, D-sub connectors feature both male and female connector orientations. Named for their resemblance to the fourth letter of the alphabet, the "D" shape ensures orientation accuracy when you join two opposing connectors. While there are a variety of plug and receptacle configurations―and some part numbers even include both male and female counterparts―be sure to designate the proper gender orientation.

2. D-sub connector types and shell size

While there are a variety of contact configurations of D-subminiature connectors, the most common are:

  •  D-Sub 9 Pin
  •  D-Sub 15 Pin
  •  D-Sub 25 Pin
  •  D-Sub 37 Pin
  •  D-Sub 50 Pin

We use the letters A through E to designate standard shell sizes for D-sub connectors. VGA connectors utilize an E-sized shell with 15 IO, which contain three rows of five contacts. When you're selecting D-sub connectors, consider both the size and the required IO for your application to ensure that you meet all communication and compactness requirements.

3. D-sub terminal pitch

The pitch between a D-sub connector's terminals allows for connector compactness. For example, a high-density 100-contact D-sub connector boasts a pitch of 0.63mm between terminals. While a lower pitch limits the contacts' allowed voltage and amperage, low-power applications containing analog or digital IO may be perfectly suited for a small-pitch D-sub connector. For higher power applications, where you might need a connector to provide power to large monitors, a higher pitch D-sub may be necessary, such as a 1.27mm or 2.54mm connector.

4. D-sub connecter voltage rating

D-sub connectors come rated for a variety of voltages. Some D-sub connectors are safely rated to carry up to 1800VAC through each contact. Connectors of this capability require high terminal pitches, such as 4.45mm, which will cause an arc discharge between terminals.

5. D-sub pin orientation

Many standard D-sub connectors, such as the well-known VGA cable, feature a "straight" body orientation. A "straight" body means that the input and output align in the same direction. Right-angle body orientation styles are commonly used in PCB-mounted applications. You can find various other body orientation styles on the market as well, including custom body orientations that let you utilize the D-sub connector in a variety of applications where space constraints may be an issue.

D-sub connectors may seem limited to legacy connector assemblies, but they are still prominent in a variety of communication applications and other connector assemblies. Their design has proven versatile and effective for nearly 70 years, and they are still utilized in a variety of connector designs. Fulfill your application's needs with anywhere from 10 to 100 IO using D-sub connectors from Arrow.com.



관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.