What is IMU? Inertial Measurement Unit Working & Applications

The term IMU stands for “Inertial Measurement Unit,” and we use it to describe a collection of measurement tools. When installed in a device, these tools can capture data about the device’s movement. IMUs contain sensors such as accelerometers, gyroscopes, and magnetometers.

How Does an IMU Work?

IMUs can measure a variety of factors, including speed, direction, acceleration, specific force, angular rate, and (in the presence of a magnetometer), magnetic fields surrounding the device.

Each tool in an IMU is used to capture different data types:

- Accelerometer: measures velocity and acceleration

- Gyroscope: measures rotation and rotational rate

- Magnetometer: establishes cardinal direction (directional heading)

IMUs combine input from several different sensor types in order to accurately output movement.

What is an IMU Used For?

You commonly see IMUs used in navigational devices or as components of navigational equipment, such as:

- Manned and unmanned aircraft. A connected (or onboard) computer can use an IMU’s measurements to calculate altitude and relative position to a reference frame, making them exceedingly useful in aircraft applications.

- GPS positioning systems IMUs serve as a supplement to GPS positioning systems, allowing the navigational device to continue with an estimated position and heading if it loses satellite connection.

Beyond their obvious applications in navigation, you can apply an IMU in nearly any field where motion detection comes into play:

- Most smartphones, tablets and fitness tracking devices contain a low-cost IMU

- IMUs are involved in sports training applications that need to measure, for example, the precise angle and force of a swing in golf or baseball.

- IMUs drive the self-balancing systems of personal transportation devices like Segways and hoverboards.

Disadvantages of IMUs

The principal disadvantage of an IMU is that they are prone to error that accumulates over time, also known as “drift.” Because the device is always measuring changes relative to itself (not triangulating against an absolute or known outside device), the IMU constantly rounds off small fractions in its calculations, which accumulate over time. Left uncorrected, these tiny imprecisions can add up to significant errors.

Still, when coupled with a corrective technology or a human operator, IMUs can be a beneficial supplement to other sensors. In precision applications, you can suspend the sensors from shock absorbers to mitigate errors as well as protect the unit.

IMU Sensors Explained

IMUs are sensing devices that incorporate at least two (and often three) types of sensors to measure a host device’s location in three-dimensional space. They are a valuable supplement to GPS or other navigational technologies. Additionally, they are present in a wide variety of consumer electronics that contain motion sensors (such as smartphones).

In most consumer applications, drift of negligible importance since an IMU doesn’t require a high degree of long-term precision. In more precise applications, users should ensure the accuracy of the sensor readings and enact occasional controls to correct for drift, especially in positioning.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.