Using an Atari Punk Console for Simple Capacitor Audio Output

게시자

Music may be an art, but making it sound its best is a science. There are many ways to produce music using both analog and digital methods, and the capacitor is one of the most critical components involved in electronic audio. Capacitors can filter out specific frequencies, they can tune a radio, and when combined with a 556 dual timer chip (or two 555 timer ICs), they can create a very simple and versatile instrument.

Simplified Stepped Tone Generator  

Fig 1: Simplified Stepped Tone Generator, also known as an Atari Punk Console 

This instrument, called a “Stepped Tone Generator,” was designed by Forrest M. Mims III and published in the 1980s. Mims’ design outputs sound signals directly to a speaker, and engineers have tweaked this simple design in countless ways, including the line-level “Atari Punk Console,” commonly used with powered speakers.

The name Atari Punk Console (APC) references the results of this build, which sound like a 1980s arcade game with their distinct bloops, bleeps, and hums. Controls consist of two potentiometer knobs: one varies the sound frequency and the other controls the width of each generated square wave.

 

Atari Punk Console DIY

Build your own Stepped Tone Generator using the parts list and instructions below

We’ve outlined a simplified version of Mims’ circuit, omitting the volume potentiometer and using a pair of CR2032 coin cell batteries to save space. We subbed 200k potentiometers for the 1M pots originally used. The parts list for this build is fairly simple, with components that are easy to find in a well-stocked shop:

1. (1) 556 timer chip (or two 555 timer ICs)

2. (2) .1μF capacitors

3. (1) 10μF capacitor

4. (2) 200 kOhm potentiometers

5. (1) 1K resistor

6. (1) 8 Ohm speaker

7. (2) CR2032 coin cell batteries and (1) holder

8. (1) Breadboard

9. Hookup Wires (single strand 22 gauge recommended)

With those parts in hand, all that’s left to do is connect the circuit as diagrammed in the image below. We recommend single-strand wire that you connect and clip to the correct length. Without clipping the wire, you’ll have a barely-visible 556 timer surrounded by a forest—pardon the pun—of unintelligible hookup wires.

 Simplified Stepped Tone Generator Layout

Fig 2: Simplified Stepped Tone Generator Layout. Capacitor connected to speaker is 10μF, others are .1μF.

This modified version shows how versatile Mims’ circuit is, and you can experiment further with different capacitor and potentiometer values. Add on to the circuit by chaining more components to its output, or by interfacing a microcontroller to change things further. You can even hook an oscilloscope to the output to see how the waveform varies as you twist the knobs.

oscilloscope with step tone generator

Fig 3: An oscilloscope can help visualize what is going on with your new instrument.

Building a Stepped Tone Generator is a fun experiment. Hearing the funky retro sounds of arcades of old is a great payoff to a correctly built circuit. While you could use a microcontroller to obtain a similar effect, this circuit is an approachable, useful introduction to both capacitors and the incredibly popular 555 and 556 integrated circuit.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.