The Benefits of Adding Cellular to Your IoT Product

Wi-Fi has typically been the most popular connectivity choice for entrepreneurs’ IoT devices. It is commonly available, provides high throughput, and is the most well-known connectivity choice for IoT, but as technology advances and costs decline, more entrepreneurs are considering adding cellular connectivity along with Wi-Fi to their creations. Read on to discover more about cellular connectivity—and why it may be the best feature to add to your IoT device.

Consistent Geographic Coverage 

Wi-Fi provides excellent coverage, but only within a very small area. When IoT devices are limited to accessing Wi-Fi only, they are tied to one location at a time, since they must be able to connect with a local Wi-Fi router in order to work. These Wi-Fi routers rarely have large reach; generally, a home router can reach up to 150 feet indoors and 300 feet outdoors. 

If you are building a device that needs to retain access to the internet no matter where the user is located, cellular connectivity is a must-have. If your IoT device has cellular connectivity, it’s very likely that customers will be able to use it the majority of the time. 

For many IoT products, cellular connectivity is critical to the product’s core function:

- Medical IoT devices, in many cases, must retain continual connectivity in case of emergency. For example, a heart monitor that can predict cardiac disturbance and send its user a warning should always be connected to the internet, no matter whether the user is near a router or not.

- Moving devices, like smart parking assistants and robot couriers, need to have consistent connectivity to function. Because they are constantly changing location, they cannot rely on a Wi-Fi router to work.

- Environmental monitoring devices also cannot rely on Wi-Fi to function properly; because they operate out of doors, Wi-Fi cannot often reach them. These devices include snow-plowing robots and earthquake sensors.

Tight Security

As anyone who has had their identity stolen in a public setting knows, public Wi-Fi is almost anyways unencrypted. Private Wi-Fi in homes is often unencrypted, too. Even if a public or private Wi-Fi system is encrypted, individuals must diligently update systems in order for them to work correctly—and it can be risky to put one’s trust in an unknown person or company. 

Cellular data is encrypted by default. Network operators hire and staff dedicated, professional cybersecurity teams specifically dedicated to monitoring and protecting your cellular network at all times, so you can be sure that your system is always operating at optimal levels. It is true that ultimately, no network can be completely secure, but cellular connectivity is the most secure option available. 

Every device that connects to the internet needs to be secure, but certain IoT devices take precedent:

- Household appliances, like smart doors, must have tight security. Otherwise, a hacker could simply disarm your system and break into your home. Alarm systems are faced with a similar problem. While in the past, price and system complexity was an issue—especially for household appliance cellular connectivity—new innovations have lowered prices and empowered users with a simpler design.

- Business appliances and applications, like smart point of sale (PoS) registers, often hold customer information such as credit card numbers and business addresses. Because they hold such valuable data, they must be secure in order to prevent identity theft and other problems. Similarly, shipping containers must be secure, lest product theft occur. 

Unquestionable Reliability

With cellular connectivity, you rarely need to worry about a weak signal or spotty connection. In the case of a power outage, as long as cell towers are functional, you don’t lose your connection at all.

This reliability that cellular connectivity provides is invaluable. It can even be considered vital to certain IoT devices, like the cardiac disturbance detection device mentioned previously, which needs to reliably function in order to provide important medical-related updates. Similarly, home appliances, like alarm systems, can’t go out during a natural disaster—in fact, this is the time you probably need them the most. 

Due to recent innovations, cellular connectivity is less expensive and more accessible than ever before. Considering that cellular connectivity offers better coverage, security, and reliability than Wi-Fi connectivity, it’s certainly worth considering for your IoT creations in the future. 

--

Considering adding cellular connectivity to your tech product?

As the Official Mobile Connectivity Provider of the Arrow Certification Program, AT&T provides exclusive tools and resources for entrepreneurs to bring their IoT products to market. Join the Arrow Certification Program today!

 

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.