ATtiny85 RGB LED Control: Addressable RGB LEDs with ATtiny85

게시자

Addressable RGB and RGBW LEDs like the famous WS2812B allow engineers to apply fantastic lighting effects on a limited budget. We explored this interesting protocol in some detail, but if you want to get things "lit," you can use the Adafruit NeoPixel library.

The NeoPixel library works well on Arduino and Adafruit boards, but what about the humble ATtiny85? Can this little chip run a bank of programmable LEDs by itself? The short answer is "yes," however, you'll need to make a few changes to get your ATtiny85 working properly.

Programming ATtiny85 RGB LED with Arduino


RGB LEDs_IMAGE 2


To get started, follow these steps:

1. Install the Adafruit NeoPixel library on the Arduino IDE, which is generally a matter of performing a search and installation via the Library Manager (through the menus or Ctrl + Shift + I)

2. Load an included example—we'll use 'strandtest' here—customizing options like the number of LEDs and which pin actually controls the chain of RGB LED modules

3. For the ATtiny85, set up the Arduino IDE (if you haven't already). Note that the chip's physical pins won't be numbered in the same way as they are in the Arduino IDE, so use this diagram for reference. If you only need one pin for LED control, Arduino IDE pin 0 (physical pin 5) is in the opposite corner of the chip's dot

4. Under 'Tools,' set the board to 'ATtiny25/45/85,' and the processor to ATtiny85

5. Select 'Internal 8 MHz' for the clock speed, as this library doesn't work at its factory settings

6. With the ATtiny85 and programmer connected, hit 'Burn Bootloader' to instruct the chip to run at this speed

A 16 MHz clock may also work, but we did not include one in our testing. Also note that depending on which LEDs you use, you may have to change some other options.


RGB LEDs_IMAGE 3-min 1


Upload and Go!

Upload the modified example code using a programmer. Connect your power and ground leads to the voltage supply and connect the signal input to the pin you assigned on the ATtiny85. With everything correctly connected, you'll see a variety of changing colors and have an extremely compact setup to control one or more addressable LEDs.

 

ATtiny85 Programming in PlatformIO

If you're using PlatformIO, as introduced here using Visual Studio Code, you can also program the ATtiny85 using this IDE. While I won't go through a step-by-step tutorial on the subject, you can review a basic piece of example code that works with it. In order to run the code, you'll need the proper library and the ATtiny85 needs to be set to run 8 MHz. I used the Arduino IDE to set the clock speed.

Finally, modify the platformio.ini file to suit your chip. You can see the configuration that worked for me in the image below:


RGB LEDs_IMAGE 4

Need an Arduino? Shop all of our Arduino products here

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.