What is Arduino Uno? An overview of Arduino’s most popular microcontroller dev board

게시자

The Arduino Uno is the poster child of development boards from the Arduino Corporation and the gold-standard prototyping tool for education and makers that require an easy-to-use microcontroller. The Arduino Uno was designed to utilize the world of microcontrollers and computer programming, but it has become the go-to first step of nearly any DIY application as it is incredibly versatile and can be used effectively by novices and pros alike.

Arduino Uno dimensions

The Arduino Uno is one of the most popular compact development boards on the market. Smaller than the palm of your hand (2.7” x 2.1”), the board is based around the removable Microchip ATmega328P microprocessor, which features 8-bit resolution and its own USB bootloader for reprogramming. With 32 KB of Flash memory, 2 KB of SRAM, and 1 KB of EEPROM, this little processor can carry out most any task you can ask of it.

The board itself holds an 16 MHz clocking quartz crystal, an USB connector, a power jack, and an ISCP header. The Arduino Uno features 20 I/O pins, with the option for six of the digital outputs to function as PWM outputs and six variable pins. See the chart below to see a detailed mapping of said pins.

Arduino Uno Pinout

Arduino Uno features and capabilities

Part of what makes the Arduino Uno so accessible to everyone is the Arduino integrated development environment (IDE). The open-source IDE uses Java to create commands and programs. From a user standpoint, the Arduino IDE contains several useful features to make codes clean and effective, such as text copy/paste and syntax highlighting. Because it’s open source, Arduino’s IDE also has an associated, community-driven library, which allows newer users to find frameworks for programs that best suit their needs and lets more experienced coders post their projects and ideas to help introduce those who are unfamiliar with the language to its syntax.

Another great facet of the Arduino Uno is the Arduino Shields. Shields are hardware add-ons that interface directly with the Uno’s pin headers and can expand its capabilities. A shield consists of a printed circuit board that has embedded components and connectors to facilitate its specific capability, and integrated software to communicate its abilities to the Uno. Shields can also be stacked on top of one another to add multiple functionalities to an Arduino Uno.

Some examples of popular Arduino shields include the Wi-Fi Shield, which gives the Uno wireless connectivity, and the Motor Shield, which allows the Uno to control DC and stepper motors. Using shields, anyone can easily integrate key functionalities to their Arduino Uno system with minimal coding and even less handiwork. Thanks to the wide repertoire of Arduino shields, almost any project can be simplified and enhanced for performance and ease of implementation.

Is the Arduino Uno right for you?

The Arduino Uno combines all the usability of a powerful microprocessor with an expansive collection of community-created software and functional shields into a very user-friendly, compact board that is great for anyone trying to get into the field of microelectronics or just trying to find an efficient way to prototype his or her idea.


관련 상품 참조

A000066 | Arduino Uno Rev3

Arduino S.r.l. Embedded System Development Boards and Kits 보기

관련 상품 참조

ATMEGA328P-PU

Microchip Technology Microcontrollers - MCUs 보기

Are you on the list?
Sign up to receive exclusive offers, product announcements, and the latest industry news.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.