3D Magnetic Sensor with Ultra-Low Power

게시자

Infineon's 3D Magnetic Sensor 2 Go Evaluation Kit is designed to familiarize users with the capabilities of a small magnetic sensor. The most important piece of hardware in the kit is the 3D Magnetic Sensor TLV493D. This sensor is highly accurate at three-dimensional sensing and consumes extremely low amounts of power. This allows tracking of 3D movement — all without requiring direct contact with the sensor.

The 3D magnetic sensor comes with several key features that make it stand out in front of other magnetic sensors.  First, the magnetic sensor consumes only 10 uA (micro-amps) in ultra-low power mode and 0.007 in power down mode! Next, the sensor comes with integrated temperature sensing , 12-bit data resoluition for the Bx, By and Bz direction up to 98 uT/LSB, and linear field measurement in all axis up to +/- 130 mT.  The sensor also comes in a standard TSOP6 package and is automatically qualified for automotive use.

The 3D Magnetic Sensor 2 GO Evaluation Kit allows almost immediate use of the magnetic sensor, right out of the box.  With both joystick and rotation nob adapters, the kit allows immediate evaluation though Infieon’s graphical user interface (GUI) which can be downloaded for free.  Additionally, the sensor is equiped with a digital I2C interface, allowing sensor and imcrocontroller bi-directional communication.

To use the GUI, simply download it from the software download page. You will also need to install a required Segger USB driver, which may be concerning to you if you are protective of the programs on your computer. Fear not, because the driver is automatically included in the Setup Wizard and will prompt you to accept their installation automatically. Once you have installed the driver and software, the GUI will be operable and you can begin evaluating the capabilities of the 3D magnetic sensor immediately.  It truly is that easy!

Mounts for the sensor’s evaluation board, which are included, a joystick and rotational knob, are automatically represented on the GUI. Simply select the tab of the mount that you have implemented and you will be able to start sensing right away.  A very creative feature that is included in the evaluation kit, is the ability to separate the sensor from the rest of the evaluation board.  This means that if you want to put just the sensor and a magnet into your controller, you can separate the sensor at the break line, solder four wires to the pin headers, and install the sensor into your own custom application.

관련 상품 참조

TLV493DA1B6HTSA2

Infineon Technologies AG Angular and Linear Position Sensors 보기

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.