Arrow Electronic Components Online

FPGA basics: architecture, applications and uses

Field Programmable Gate Arrays - FPGAs09 may 2024
A person holds a tablet displaying data while overseeing a robotic arm assembling a car frame in a modern factory.
View all articles

The Field Programmable Gate Array (FPGA) is an integrated circuit that consists of internal hardware blocks with user-programmable interconnects to customize operation for a specific application.

What is FPGA?

Field Programmable Gate Array (FPGA) is an integrated circuit that consists of internal hardware blocks with user-programmable interconnects to customize operation for a specific application. The interconnects can readily be reprogrammed, allowing an FPGA to accommodate changes to a design or even support a new application during the lifetime of the part.

The FPGA has its roots in earlier devices such as programmable read-only memories (PROMs) and programmable logic devices (PLDs). These devices could be programmed either at the factory or in the field, but they used fuse technology (hence, the expression “burning a PROM”) and could not be changed once programmed. In contrast, FPGA stores its configuration information in a re-programmable medium such as static RAM (SRAM) or flash memory. FPGA manufacturers include Intel, Lattice Semiconductor, Microchip Technology and Microsemi.

FPGA architecture

A basic FPGA architecture (Figure 1) consists of thousands of fundamental elements called configurable logic blocks (CLBs) surrounded by a system of programmable interconnects, called a fabric, that routes signals between CLBs. Input/output (I/O) blocks interface between the FPGA and external devices.

Depending on the manufacturer, the CLB may also be referred to as a logic block (LB), a logic element (LE) or a logic cell (LC).

This image displays a schematic block diagram of an FPGA architecture, highlighting its main components. The diagram features labeled sections for Logic Blocks, I/O Blocks, and Programmable Routing, each shown in detail with circuit symbols. The central grid structure is surrounded by input/output connections, illustrating the modular and reconfigurable nature of the device.

The fundamental FPGA architecture (Image Source: National Instruments)

Figure 1

An individual CLB (Figure 2) is made up of several logic blocks. A lookup table (LUT) is a characteristic feature of an FPGA. An LUT stores a predefined list of logic outputs for any combination of inputs: LUTs with four to six input bits are widely used. Standard logic functions such as multiplexers (mux), full adders (FAs) and flip-flops are also common.

A detailed block diagram of a logic cell, featuring two 3-LUT (three-input look-up tables), a full adder (FA), and a D flip-flop (DFF). The diagram illustrates the flow of signals such as 'carry in', 'carry out', and 'clk', as well as the use of multiplexers (mux) to route signals. Key numeric concepts like '3-LUT' and 'DFF' are explicitly labeled, and the diagram is annotated with circled numbers for reference.

A simplified CLB: The four-input LUT is formed from two three-input units. (Image source: Wikipedia)

Figure 2

The number and arrangement of components in the CLB varies by device; the simplified example in Figure 2 contains two three-input LUTs (1), an FA (3) and a D-type flip-flop (5), plus a standard mux (2) and two muxes, (4) and (6), that are configured during FPGA programming.

This simplified CLB has two modes of operation. In normal mode, the LUTs are combined with Mux 2 to form a four-input LUT; in arithmetic mode, the LUT outputs are fed as inputs to the FA together with a carry input from another CLB. Mux 4 selects between the FA output or the LUT output. Mux 6 determines whether the operation is asynchronous or synchronized to the FPGA clock via the D flip-flop.

Current-generation FPGAs include more complex CLBs capable of multiple operations with a single block; CLBs can combine for more complex operations such as multipliers, registers, counters and even digital signal processing (DSP) functions.

CPLD vs FPGA

Originally, FPGAs included the blocks in Figure 1 and little else, but now designers can choose from products with a large range of features. Less complex devices such as simple programmable logic devices (SPLDs) and complex programmable logic devices (CPLDs) bridge the gap between discrete logic devices and entry-level FPGAs.

Entry-level FPGAs emphasize low power consumption, low logic density and low complexity per chip. Higher-function devices add functional blocks dedicated to specific functions: Examples include clock management components, phase-locked loops (PLLs), high-speed serializers and deserializers, Ethernet MACs, PCI express controllers and high-speed transceivers. These blocks can either be implemented with CLBs—termed soft IP—or designed as separate circuits; i.e., hard IP. Hard IP blocks gain performance at the expense of reconfigurability.

At the high end, the FPGA product family includes complex system-on-chip (SoC) parts that integrate the FPGA architecture, hard IP and a microprocessor CPU core into a single component. Compared to separate devices, a SoC FPGA provides higher integration, lower power, smaller board size and higher-bandwidth communication between the core and other blocks.

SoC FPGAs

SoC FPGAs include a wide range of processing capabilities to suit different applications. A low-cost, low-power SoC FPGA such as Intel’s Cyclone V, for example, targets high-volume applications such as industrial motor control drives, protocol bridging, video processing cards and handheld devices. The device (Figure 3) has two distinct parts: the FPGA portion and a hard processor system (HPS) based around a single- or dual-core 32-bit Arm Cortex-A9 MPCORE running at 925 MHz. Each part contains its own set of peripherals, which includes hard IP from third-party vendors.

This diagram illustrates the architecture of the Intel Cyclone V SoC FPGA, divided into HPS and FPGA portions. The HPS portion includes components such as Flash Controllers, SDRAM Controller Subsystem, Cortex-A9 MPU Subsystem, and more. The FPGA portion features elements like Control Block, User I/O, HSSI Transceivers, FPGA Fabric, and Hard PCIe. The diagram visually separates the two main sections and highlights their respective subsystems and interfaces.

The Cyclone V SoC internal block diagram (Image Source: Cornell University)

Figure 3

At the other end of the scale, the Stratix 10 SX targets high-performance applications in communications, data center acceleration, high-performance computing (HPC), radar processing and ASIC prototyping; that FPGA includes a quad-core 64-bit Arm Cortex-A53 running at up to 1.5 GHz.

FPGA design

How do we transform this collection of thousands of hardware blocks into the correct configuration to execute the application? An FPGA-based design begins by defining the required computing tasks in the development tool, then compiling them into a configuration file that contains information on how to hook up the CLBs and other modules. The process is similar to a software development cycle except that the goal is to architect the hardware itself rather than a set of instructions to run on a predefined hardware platform.

Designers have traditionally used a hardware description language (HDL) such as VHDL (Figure 4) or Verilog to design the FPGA configuration.

VHDL code implementing a signed adder entity and architecture. The code includes ports for aclr, clk, a, b, and q, with signal processing and assertion for vector length. Numeric values such as '1164' and '35' are visible in the code lines and library references. Syntax highlighting distinguishes keywords, variables, and comments.

Sample VHDL code for a signed adder (Image Source: Wikipedia)

Figure 4

Once the FPGA design has been created and verified using HDL, the compiler takes the text-based file and generates a configuration file that contains information on how the components should be wired together. Even if the HDL code has no errors, choosing the wrong FPGA may still cause the compilation to fail—for example, the FPGA runs out of a specific resource type or the compiler cannot create the required routes between components.

One challenge with an HDL approach is that configuring an FPGA requires both coding skills and a detailed knowledge of the underlying hardware, and the required expertise is not widely available.

As a result, vendors are offering software development kits (SDKs) that allow designers to develop FPGA solutions in popular high-level languages such as C/C++, Python and OpenCL. High-level synthesis (HLS) design tools are also available; these run on a framework such as National Instrument’s LabVIEW and feature graphical block diagrams instead of lines of code.

FPGA uses: An attractive choice for certain applications

The ability to configure the hardware of the FPGA, reconfigure it when needed and optimize it for a particular set of functions makes the FPGA an attractive option in many applications.

FPGAs are often used to provide a custom solution in situations in which developing an ASIC would be too expensive or time-consuming. An FPGA application can be configured in hours or days instead of months. Of course, the flexibility of the FPGA comes at a price: An FPGA is likely to be slower, require more PCB area and consume more power than an equivalent ASIC.

Even when an ASIC will be designed for high-volume production, FPGAs are widely used for system validation, including pre-silicon validation, post-silicon validation and firmware development. This allows manufacturers to validate their design before the chip is produced in the factory.

FPGA applications

Many applications rely on the parallel execution of identical operations; the ability to configure the FPGA’s CLBs into hundreds or thousands of identical processing blocks has applications in image processing, artificial intelligence (AI), data center hardware accelerators, enterprise networking and automotive advanced driver assistance systems (ADAS).

Many of these application areas are changing very quickly as requirements evolve and new protocols and standards are adopted. FPGAs enable manufacturers to implement systems that can be updated when necessary.

A good example of FPGA use is high-speed search: Microsoft is using FPGAs in its data centers to run Bing search algorithms. The FPGA can change to support new algorithms as they are created. If needs change, the design can be repurposed to run simulation or modeling routines in an HPC application. This flexibility is difficult or impossible to achieve with an ASIC.

Other FPGA uses include aerospace and defense, medical electronics, digital television, consumer electronics, industrial motor control, scientific instruments, cybersecurity systems and wireless communications.

FPGA history: What comes next?

With these emerging applications, the FPGA market is growing at a healthy clip: It was valued at $5.34 billion in 2016 and is expected to grow to $9.50 billion in 2023, according to industry researchers MarketsandMarkets. That’s a compound annual growth rate (CAGR) of 8.5 percent, compared to a CAGR of about 2 percent for the much larger ($74 billion) general microprocessor market.

The exponential growth of data, and the emergence of fast-changing fields such as AI, machine learning, HPC and genomics, require architectures that are fast, flexible and adaptable. FPGAs are well-positioned to take advantage of these new opportunities.

Etiquetas de artículo

Dispositivos Programables
Matrices de Puerta Programables en Campo - FPGAs
Inteligencia Artificial (AI)
Aprendizaje Automático