Selecting quartz crystals and oscillators for dependable industrial and automotive performance
A quartz timing device is one of the least expensive parts on most bills of material and one of the easiest to under-specify. The frequency on the label is only part of the picture.
Real accuracy depends on initial tolerance, drift over temperature, first-year aging, supply and load variation, and how well a crystal is matched to the oscillator circuit driving it. When one of those factors is missed, the symptoms appear late and are expensive to chase: a radio that fails to associate at temperature extremes, a clock that drifts minutes across a year, or a start-up failure in a fraction of a production lot. Sourcing adds a second set of constraints. A product family spanning several supply rails, temperature grades, and frequencies can accumulate a long list of timing part numbers, each with its own qualification and forecast. ECS Inc. International addresses both concerns with a portfolio that runs from cost-effective tuning fork crystals through low-jitter oscillators and temperature-compensated devices, much of it built on a MultiVolt™ architecture that lets one device operate across a range of supply voltages.
Matching the Device Class to the Requirement
A crystal is a passive resonator. It sets the frequency but depends on the oscillator circuit inside the microcontroller or transceiver, which makes load capacitance, equivalent series resistance, and drive level part of the design work. Insufficient negative resistance margin is a common cause of intermittent start-up problems and is best checked during design rather than after a build. An oscillator packages the resonator with its own circuit and supplies a defined output with a specified jitter figure. A TCXO adds temperature compensation and holds accuracy in the sub-ppm range where an uncompensated crystal would drift by tens of ppm.
Selection usually starts with the total stability budget. Initial tolerance at 25°C, stability across the operating range, and first-year aging should be added together and compared against the tightest system requirement, whether that is a wireless channel raster, a SerDes reference clock, or a timekeeping function that must stay accurate between synchronizations. From there, designers confirm load capacitance and ESR for crystals, output type and jitter for oscillators, and supply voltage for both. Environmental requirements set the temperature grade and whether AEC-Q200 qualification is needed, and package size often decides the final choice in dense assemblies. Devices that cover several supply voltages and use industry-standard footprints reduce the number of part numbers a team carries.
Application Examples
Computers, peripherals, and IoT devices. Sleep-mode timekeeping runs on a 32.768 kHz reference. The ECX-31B is a tuning fork crystal in a 3.2 x 1.5 x 0.9 mm two-pad package, with ±20 ppm standard tolerance and a ±10 ppm option, 70 kΩ maximum ESR, and load capacitance choices of 6, 7, 9, and 12.5 pF across -40°C to +85°C. ECS rates drive level for its tuning forks at roughly 0.1 µW against about 10 µW for most AT-cut crystals, which is why this class anchors low-power clocking in battery-operated products.
Communications and networking equipment. Wired and wireless links need a MHz reference that stays inside a tight window for the life of the product. The ECX-2236B is a 2.5 x 2.0 x 0.55 mm surface-mount crystal with ±10 ppm tolerance at 25°C, stability options from ±10 ppm to ±20 ppm depending on the temperature range, low ESR, and first-year aging of ±1 ppm maximum. Low aging matters in equipment that will not be recalibrated in the field.
Test equipment and high-speed data paths. Serial links, data converters, and FPGA fabrics are sensitive to reference jitter. The ECX2-LMV is an LVDS MultiVolt™ oscillator with sub-50 fs RMS phase jitter from 12 kHz to 20 MHz at 156.25 MHz, ±25 ppm stability over -40°C to +85°C, a 2.375 V to 3.63 V supply, and 24 mA maximum current, at reference frequencies including 100 MHz, 125 MHz, and 156.25 MHz. That supply range lets one device serve 2.5 V and 3.3 V designs.
Medical devices and portable wireless. Where frequency accuracy governs link performance and current budget is tight, a compensated device earns its place. The ECS-TXO-20CSMV is a clipped sine wave TCXO in a 2.0 x 1.6 x 0.8 mm package, covering 10 MHz to 52 MHz with ±0.5 ppm stability in the AY option, MultiVolt™ supply support, and roughly 2.0 mA current consumption.
Automotive and transportation. Under-hood and in-cabin electronics face shock, vibration, and temperature extremes. The ECX-1637QZ is a 2.0 x 1.6 x 0.45 mm crystal covering 16 MHz to 60 MHz over -40°C to +125°C, with AEC-Q200 compliance, which suits automotive assemblies and other harsh-environment designs where mechanical stress is a design factor.
ECS Timing Solutions from Arrow
ECS supports selection with design tools rather than datasheets alone. Its published calculators cover crystal load capacitance, ppm to Hz conversion, and frequency stability over time, the last of which estimates how tolerance and temperature variation translate into clock drift across a service life. ECS also publishes material on negative resistance margin and on MultiVolt™ operation, both useful when moving from a first schematic to a design that starts reliably across a production lot.
Arrow stocks the ECS crystal, oscillator, and TCXO families to support designs from prototype through volume production.
Article tags