Precision timing for stable clock signals in harsh operating environments
Every clocked system depends on a reference oscillator that maintains its frequency as operating conditions change. Timing devices deployed in harsh environments may need to withstand vibration from motors and road surfaces, sudden airflow from cooling fans, rapid temperature swings, board flex, and electromagnetic noise from nearby switching circuits.
If these stressors are not properly accounted for, timing variation can contribute to synchronization challenges, system-level performance issues, or late-stage compliance work. Quartz oscillators remain widely used across the electronics industry and continue to be a practical choice for many applications. However, some designs require tighter stability, greater resilience to environmental stress, smaller form factors, or more flexible sourcing options than traditional quartz timing architectures can provide. In telecom, automotive, industrial, and portable equipment, these requirements increasingly influence how engineers evaluate precision timing solutions.
Precision Timing and Environmental Stress
The SiTime devices described here are part of the company's programmable oscillator families. These oscillators use a silicon MEMS resonator as the frequency reference, while CMOS circuitry maintains oscillation and synthesizes the output. The resonator carries very little mass, which can help it hold frequency under vibration and shock, and it is sealed in a vacuum cavity at the wafer level. The wider SiTime catalog also includes clock generators, buffers, jitter cleaners, and network synchronizers, so the characteristics here apply to the families named below rather than to the whole line.
Selected Super-TCXO and OCXO families, including the SiT5356, SiT5811, and ENDR-TTT, use DualMEMS® temperature sensing and TurboCompensation®, which track resonator temperature closely and correct frequency during fast thermal transients such as those caused by airflow. Programmability is a second characteristic, and its scope is device dependent: frequency, stability, supply voltage, drive strength, spread-spectrum modulation, and digital frequency pulling are configurable on some families and fixed on others, so the datasheet for a given part defines what can be adjusted and which combinations can be ordered. Where a device meets the design's electrical and mechanical requirements, its configurability can reduce the number of timing part numbers a team must qualify and stock.
What to Evaluate When Selecting Precision Timing
Selection typically starts with performance and application fit: frequency stability over temperature, jitter and phase noise limits for high-speed links, supply voltage, and, for network equipment, holdover behavior when an upstream reference is lost. Designers should also consider environmental and mechanical reliability, including the required temperature range, qualification standards such as AEC-Q100, and exposure to shock, vibration, and airflow. Availability and lifecycle confidence carry equal weight, since programmable parts with short lead times help keep production schedules predictable. It is also worth confirming which combinations of stability, temperature range, package, and voltage are orderable, since the limits quoted across a datasheet are rarely available in one configuration.
Application Examples
Communications infrastructure. Many telecom and data center systems must stay synchronized, and some must hold accurate time if a reference drops out. The SiT5356 Super-TCXO supports any frequency from 1 to 60 MHz with stability options of ±0.1, ±0.2, and ±0.25 ppm, and it is fully compliant with Telcordia GR-1244-CORE Stratum 3 oscillator specifications. On the high-speed data path, the SiT9501 differential oscillator delivers 70 fs typical RMS phase jitter at 14 standard networking frequencies from 25 MHz to 644.53125 MHz, in packages down to 2.0 x 1.6 mm.
Automotive. Advanced driver assistance, infotainment, and body electronics see vibration and wide temperature ranges. The AEC-Q100 qualified SiT8924 covers 1 to 110 MHz, with stability options of ±20, ±25, ±30, and ±50 ppm and temperature options reaching -55°C to +125°C. It is offered in five industry-standard packages, from 2.0 x 1.6 mm to 7.0 x 5.0 mm, matching footprints already used for quartz oscillators. The ordered part number sets which combination applies.
IoT, edge, medical, and portable devices. Battery-powered products need a MHz clock that uses as little current and board area as possible. The SiT8021 operates from 1 to 26 MHz in a 1.5 x 0.8 mm package with ±50 or ±100 ppm stability, drawing 60 µA at 3.072 MHz with a standby mode at 0.7 µA typical. Frequencies are factory programmed, so one device family can support several variants of a wearable, medical monitor, or IoT sensor node.
Industrial automation and electronics. Motor drives, displays, and high-speed serial links generate emissions that must be managed at the system level. The SiT9005 spread-spectrum oscillator covers 1 to 141 MHz with selectable center or down spread and eight rise and fall time options. SiTime reports EMI reductions of up to 17 dB at the carrier frequency and up to 30 dB on harmonics. Results depend on the board, so engineers generally test settings in the system before fixing a configuration.
SiTime Precision Timing Solutions from Arrow
Arrow carries SiTime precision timing devices for each of the applications above. Network synchronization is served by the SiT5356 and SiT5358 Super-TCXOs and by the SiT5811, an Epoch Platform OCXO with ±1 ppb stability and up to 12 hours of holdover. Automotive, high-temperature, and ruggedized designs draw on the SiT8924, SiT8918, SiT8944, and SiT5346. Low-power designs use the SiT8021, SiT1602, and SiT2001; differential clocking uses the SiT9120 and SiT9501; and the SiT9005 covers EMI-sensitive designs. For ruggedized precision timing, the Endura ENDR-TTT Super-TCXO offers factory-programmed frequencies from 1 to 105 MHz, ±50 ppb to ±500 ppb stability over temperature, 0.004 ppb/g acceleration sensitivity, and operation from -55°C to +125°C.
The SiTime Time Machine II Programmer lets engineers configure field-programmable oscillators to exact frequency, voltage, stability, spread-spectrum, and drive-strength requirements for prototyping within seconds. When paired with compatible designs and appropriate qualification, SiTime's programmable timing portfolio can help engineering and purchasing teams move from design to volume production with confidence.
Article tags