Arrow Electronic Components Online

Mastering The Next-Generation of Automotive Lighting Design in Zonal Architectures

Automotive Lighting Design29 Jan 2026
A detailed view of a blue car's front headlight and LED daytime running light, both illuminated.
View all articles

The automotive industry is rapidly transitioning from domain-based to zonal architectures. Driven by the need to reduce wiring harness weight and support Software-Defined Vehicles (SDVs), this evolution utilizes a high-speed Ethernet backbone to connect distinct physical zones. This centralization allows for a “smart brain” capable of complex decision-making to be decoupled from the immediate hardware, facilitating over-the-air (OTA) updates and supporting advanced autonomous functions through more seamless sensor fusion.

However, as the central compute becomes faster and the backbone shifts to Ethernet, a new challenge emerges at the periphery of the network: the “edge.” The number of edge nodes, such as sensors, motor actuators, and lighting modules, is increasing to meet user expectations for safety, enhanced feedback, and the end-user experience.

Block diagram illustrates the connection between an Ethernet end point and multiple smart edge nodes.

If these edge systems create a data bottleneck, it can undermine the speed and efficiency of the zonal design. To fully unlock the potential of this architecture, the industry requires solutions that ensure the vehicle’s functional endpoints are as fast and responsive as its central computing core.

The Evolving Role of Automotive Lighting

The pressure on the edge of a zonal network is a direct result of changing vehicle functionality, with lighting representing a major area of significant evolution. Automotive lighting has evolved far beyond its traditional role of simple illumination to become a critical element of vehicle design, communication, and safety. Modern vehicles now demand lighting systems that not only serve as critical feedback mechanisms but also as a social interface.
 
Automotive OEMs now deploy thousands of LEDs capable of high-speed, dynamic animations for exterior signaling, branding, and safety warnings, as well as seamless ambient lighting environments inside the cabin. Furthermore, this trend is only set to expand with numerous other lighting deployments shifting from static illumination to active communication surfaces. This transformation is already entering service in the Chinese market, where early adopters are utilizing high-resolution matrix panels to project symbols and text to pedestrians.
To meet the stringent functional, aesthetic, and safety demands of modern vehicles, lighting systems must satisfy the following core technical requirements:

  • Standard Functional Applications: Simple localized tasks, such as in-cabin lights or applications like charging port indicators, require cost-effective, reliable control without excessive bandwidth, and that can connect to the zonal architecture.
  • High-Dynamic Applications: OEMs are increasingly deploying advanced animated exterior lighting, communicative light bars, and high-resolution interior displays that require the high-speed and accurate synchronization of thousands of LEDs.
  • Safety Criticality: For specific use cases, such as turn signals or autonomous driving status indicators, systems must adhere to rigorous functional safety standards, requiring ASIL compliance to ensure they function correctly when needed.
  • Reliability & Robustness: Automotive environments are harsh. Lighting systems must maintain consistent performance despite electromagnetic interference (EMI), temperature fluctuations, and the physical stresses of the vehicle environment.

For OEMs, while automotive LED design is a multifaceted challenge, scalability is arguably the key concern. Automotive designers need to integrate this vast variation of lighting functions into the zonal architecture without exponentially increasing design complexity. This requires intelligent lighting nodes that can handle specific functions efficiently while communicating seamlessly with the central zonal controller.
 
However, traditional automotive communication protocols are increasingly becoming a bottleneck. Standard LIN, with its low bandwidth and limited node count, is insufficient for dynamic arrays, and manufacturers are often challenged by the protocol’s restriction on slave addresses per cluster. Similarly, traditional CAN networks, while outperforming LIN, still struggle with the latency and protocol overhead required for fluid, high-speed animations across large matrices. To bridge the gap between the high-speed Ethernet endpoint and these demanding edge applications, a different approach is required.

The High-Speed Enabler: MeLiBu® 2.0 and Zonal Architectures

While hardware integration is crucial for zonal architectures, effective communication and software design are equally critical. For high-dynamic lighting applications, such as illuminated grilles, dynamic rear lamps, and full-width dashboard illumination, within zonal vehicle platforms, standard automotive protocols fall short.
 
To resolve this bottleneck, Melexis developed MeLiBu® (Melexis Light Bus), a communication protocol optimized for LED Driver ICs. The latest evolution, MeLiBu® 2.0, has been specifically engineered to meet the latest lighting demands, including dynamic matrix lighting displays and support high-speed zonal architectures.
 
MeLiBu® 2.0 is a UART over CAN interface that leverages the robust differential bus of CAN-FD, ensuring resilience against the electrical noise and interference common in long zonal wiring harnesses, while providing the simplified protocol handling of UART. Unlike standard CAN, MeLiBu® 2.0 is optimized for speed, supporting bandwidths of up to 4 Mbit/s. This speed is critical for modern zonal architectures where the central computer controls complex lighting patterns and “streams” them to the edge nodes in real-time.
 
Furthermore, its efficient data packaging ensures that most of the available bandwidth is devoted to transmitting actual lighting information rather than protocol overhead, allowing real-time, dynamic lighting animations to run smoothly across large, multi-segment installations without delays or performance degradation.
 
To facilitate this, MeLiBu® 2.0 is designed to connect seamlessly to the zonal backbone via standard 10BASE-T1S Ethernet endpoint bridges, translating high-speed Ethernet traffic directly to the local bus. This allows the vehicle’s lighting arrays to possess animated control more like a video screen than a set of static bulbs, enabling fluid animations without latency or visual artifacts.

This diagram illustrates the implementation of Ethernet endpoints within an automotive lighting system.

MeLiBu® 2.0 is built for the scale that modern OEMs require. As vehicles integrate more feedback mechanisms into the exterior and interior, the number of nodes per zone rises significantly. MeLiBu® 2.0 supports up to 251 nodes on a single bus, enabling the deployment of more than 4,000 RGB LEDs (or 24,000 single-color LEDs) on a single interface. This scalability ensures that even massive external matrix panels or extensive ambient lighting strips can be driven without requiring fragmented sub-networks or complex wiring workarounds.
 
The shift toward “surface lighting” and communicative LED arrays is perhaps the clearest example of where traditional architectures fail and Zonal approaches succeed. In exterior lighting, manufacturers are moving from simple clusters to high-resolution display panels capable of displaying symbols and text.

Hardware Integration and Creating a Code-Free Edge

If the Zonal architecture relies on MeLiBu® 2.0 to solve the data bottleneck, the second critical pillar for automotive designers is managing the sheer complexity of connecting thousands of individual LEDs. This challenge requires innovation at the IC and firmware level to ensure reliability, compactness, and simplified software management.
 
Fail-Safe Design
 
In high-node count applications, a major concern is single-point failure, where the malfunction of one component takes the entire chain down. Many LED driver circuits still rely on a basic daisy-chain internal bus design for the ICs, which means a physical failure on the chip’s electronic path could interrupt data flow to every subsequent node.
 
Melexis LED driver ICs address this integration risk by incorporating an internal bus design. Unlike a traditional daisy-chain, each IC in this architecture is connected in a way that ensures a failure in one LED driver does not compromise the functionality of other nodes in the series. For OEMs, this design translates directly into long-term reliability and robustness in complex lighting modules, simplifying diagnostic and maintenance strategies.
 
To support safety-critical applications, all MeLiBu® 2.0 drivers also facilitate ASIL B Safety Element out of Context (SEooC) compliance, including configurable fail-safe scenarios stored directly on the IC. This ensures that warning signals, emergency lights, and other critical lighting functions remain operational even under challenging conditions or partial system failures. These benefits extend across strings or matrices with thousands of LEDs, making the ICs suitable for both interior and exterior safety-critical lighting applications.
 
Furthermore, ICs that support cross-free PCB layouts, such as the MLX80142 series, further streamline integration by accommodating ultra-low profile designs through compact manufacturing methods like PCB-less over-molding through Injection Molded Structural Electronics (IMSE).
 
The Power of Code-Free End Points in Zonal Architectures
 
The move toward software-defined vehicles relies on endpoints that can be addressed directly by the central system, placing increased importance on streamlined and standardized hardware at the edge. While Melexis continues to support traditional Flash-programmable LED drivers for highly customized implementations, the company also offers a range of Code-Free drivers. For many typical lighting applications, particularly in projects where software development effort or in-house software expertise is limited, these Code-Free solutions provide a simplified and cost-effective path to integration within zonal architectures.
 
As a result, OEMs deploying zonal architectures look to ensure that intelligence resides only in the central supercomputer, minimizing the need for software at the edge. This preference is met by Melexis’ “Code-Free” LED drivers, which come equipped with configurable firmware featuring validated application functions, allowing for sophisticated lighting control through simple state changes rather than microcontrollers (MCUs) running custom firmware.
 
Melexis “Code-Free” drivers are designed to provide a number of operational and development benefits aligned with zonal architectures:

  • Avoiding Software Development: Engineers can define lighting sequences, calibration, and diagnostics using an intuitive Graphical User Interface (GUI), eliminating time-consuming firmware development and validation at the component level, which is crucial for managing the qualification costs associated with complex zonal systems.

A computer screen displays an LED RGB control software interface, featuring a color wheel, sliders for RGB values, and various configuration options.

  • Security by Design: Removing custom software from the edge reduces the vulnerable attack surface for exploitation, making the node inherently more robust against cyber threats than a traditional flash-configured device.
  • Decoupling Complexity: This architecture allows the central controller to be fully software-defined while the nodes remain strictly hardware-defined, streamlining the entire vehicle development cycle by aligning the hardware function exactly with the architectural philosophy of the zonal controller.

Hybrid Zonal Networks: Essential Solutions for LIN and Actuation

While MeLiBu® 2.0 provides the crucial high-speed interface for lighting communication, the reality of zonal architectures is that they are hybrid networks requiring multiple communication standards. Beyond its MeLiBu® offering, Melexis also provides a wide range of LIN LED drivers for simple, cost-effective deployments such as ambient light strips, simple reading lights, and charge port indicators.
 
To further aid LIN deployment in Zonal Architectures, where integration constraints are severe, Melexis provides specialized solutions like the MLX81120 LIN Slave Extender (often referred to as a LIN gateway).
 
This device is crucial for overcoming limitations where the number of LIN node addresses are insufficient for the vehicle’s designed functionality. The LIN extender allows designers to securely and reliably expand the local LIN bus network without adding complexity to the central zonal controller.
 
Case Study: The Smart Charging Port: Ensuring Intelligent Operation and System Simplicity
 
This integration challenge is nowhere more apparent than at the EV charging port, where numerous safety and feedback mechanisms must operate via a single connection point.

Conclusion: Building the Future of Software-Defined Light

The transition to zonal architectures is inevitable, but its success relies on the performance of the edge. As vehicles become defined by software, the hardware at the extremities must become faster, smarter, and easier to integrate.
 
Melexis provides the missing link in this evolution. By combining the high-speed data capabilities of MeLiBu® 2.0 with the architectural simplicity of Code-Free drivers and robust LIN solutions, OEMs can resolve the zonal data bottleneck. This ensures that the functional endpoints of the vehicle are as agile as its central computer, delivering the safety, communication, and aesthetic features that define the next generation of mobility.

Article tags

Automotive
LED Lighting
Melexis