The challenge of designing robust electronic circuitry often results in a design with a multitude of discrete protection components with associated cost, design time and space additions. This article discusses the fault protected switch architecture, along with the performance benefits and other advantages it offers versus traditional discrete protection solutions. A new novel switch architecture and proprietary high voltage process which provides industry leading fault protection along with the performance required for precision signal chains is discussed. ADI’s new portfolio of fault protected switches and multiplexers (ADG52xxF and ADG54xxF) use this technology.
Analog input protection for high performance signal chains is often a pain point for system designers. There is typically a significant tradeoff between analog performance (leakage, on resistance, etc) and the level of protection that can be offered by discrete components.
Replacing the discrete protection components with overvoltage protected switches and multiplexers can offer significant benefits in terms of Analog performance, robustness and solution size. The overvoltage protected component sits between sensitive downstream circuitry and the input that is exposed to external stresses. An example of this would be the sensor input terminal in a process control signal chain.
This article details the issues caused by overvoltage events, discusses traditional discrete protection solutions and the associated drawbacks, presents the solution offered by overvoltage protected analog switches including features and system benefits, and finally introduces the industry leading portfolio of ADI fault protected analog switches.
Overvoltage Issues – Back to Basics
When the input signal applied to a switch exceeds the power supplies (VDD or VSS) by more than a diode drop, the ESD protection diodes within the IC become forward biased and current flows from the input signal to the supplies, as shown in Figure 1. This current could damage the part and may trigger a latch-up event if the current is not limited
.png?h=228&&w=500?mw=290&hash=B6F7199D75C2FCE5F73EFA2C2568505D)
Figure 1. Overvoltage current path
If the switch is unpowered, there are a couple of scenarios that could occur:
1. If the power supplies are floating, the input signal could end up powering the VDD rail through the ESD diodes. In that case the VDD pin goes to within a diode drop of the input signal. This means the switch would effectively be powered, as would any other components using the same VDD rail. This could lead to unknown and uncontrolled operation of devices in the signal chain.
2. If the power supplies are grounded, the PMOS device will turn on with negative VGS so the switch will pass a clipped signal to the output, possibly damaging downstream components which would also be unpowered (see Figure 2). Note: if there are diodes to the supply, they will forward bias and clip the signal to +0.7V.
.png?h=379&&w=700?mw=290&hash=CF17D84787BD06E95EE30334A371DF05)
Figure 2. Overvoltage signal with power supply grounded
Discrete Protection Solution
Designers traditionally solve input protection issues with discrete protection components.
Large series resistors are used to limit the current during a fault, and shottky or zener diodes to the supply rails clamp any overvoltage signals. An example of such a protection scheme in a multiplexed signal chain is shown in Figure 3.
However, there are many disadvantages to using these discrete protection components.
1. The series resistor will increase the settling time of the multiplexer and slow down the overall settling time.
2. The protection diodes will introduce additional leakage current and varying capacitance which will impact the precision and linearity of the measurement
3. There will be no protection in the floating supply condition as the ESD diodes to the supplies won’t provide any clamping protection.
.png?h=196&w=700?mw=290&hash=70CD4CA0429602312D8F878AEE03B06E)
Figure 3. Discrete protection solution
Traditional Switch Architecture
The diagram in Figure 4 gives an overview of a traditional switch architecture. The switch component (on the right hand side of Figure 4) has ESD diodes to each of the supply rails, at both the input and output side of the switch element. The external discrete protection components are shown here as well – the series resistor for current limiting and the shottky diodes to the supplies for overvoltage clamping. There is often a requirement for a bidirectional TVS for additional protection in harsher environments.
.png?h=304&w=700?mw=290&hash=5138DC9E91DCF4F9E748C4070E4754DA)
Figure 4. Traditional switch architecture with external discrete protection
Fault Protected Switch Architecture
The fault protected switch architecture is shown in Figure 5. The ESD diodes at the input side are replaced with a bi-directional ESD cell, so the input voltage range is no longer limited by the ESD diodes to the supply rails. Therefore the input can see voltages up to the limitation of the process (which is +/-55V for the new fault protected switches from ADI).
The ESD diodes remain at the output side in most cases as there usually isn’t a requirement for overvoltage protection from the output side.
The ESD cell at the input side can still provide excellent ESD protection. The ADG5412F overvoltage fault protected quad SPST switch which uses this type of ESD cell achieves a 5.5kV HBM ESD rating.
There may still be a requirement for an external TVS or a smaller current limiting resistor for more stringent cases such as IEC ESD (IEC 61000-4-2), EFT, or surge protection.
.png?h=355&w=700?mw=290&hash=733BD318F225649F450BDFB3ED4F5387)
Figure 5. Fault protected switch architecture
In the case of an overvoltage condition at one of the switch inputs, the affected channel turns off and the input goes high impedance. The leakage will remain low on the other channels so the remaining channels can continue to operate as normal with minimal impact on performance. This allows for very little compromise between system speed/performance and overvoltage protection.
The fault protected switch can therefore greatly simplify the signal chain solution. The switch overvoltage protection removes the requirement for the current limiting resistors and Schottky diodes in many cases. The overall system performance is no longer limited by external discrete components which typically introduce leakage and distortion into a signal chain.
ADI Fault Protected Switch Features
The new portfolio of fault protected switches from ADI are built on a proprietary high voltage process which provides overvoltage protection up to +/-55V in both the powered and unpowered states. These parts provide industry leading performance for fault protected switches for precision signal chains.
Latchup Immunity
The proprietary high voltage process is also trench isolated. An insulating oxide layer is placed between NDMOS and the PDMOS transistors of each switch. Parasitic junctions, which occur between the transistors in junction-isolated switches, are eliminated and the result is a switch that is latch-up immune under all circumstances. The ADG5412F for example passes JESD78D latch-up test of +/-500mA for 1 second pulse width, which is the most stringent test in the specification.
.png?h=360&&w=400?mw=290&hash=8A3B00CED7DCDAAB757923D21E742758)
Figure 6. Trench isolated process
Analog Performance
As well as achieving industry leading robustness (overvoltage protection, high ESD rating, known state at powerup without digital inputs present), the new ADI fault protected switches also have industry leading analog performance. Switch performance as always is a tradeoff between low on resistance and low capacitance/charge injection. The choice of switch usually depends on whether the load is high impedance or low impedance.
Low Impedance Systems
Low on resistance parts are usually used in low impedance systems, where the on resistance of the switch needs to be kept to a minimum. In a low impedance systems such as a power supply or gain stage, the on resistance and source impedance in parallel with the load can cause gain errors. Even though gain errors can be calibrated out in many cases, the variation of on-resistance (RON) across signal range or between channels produces distortion which cannot be calibrated out. Therefore low resistance circuits are more subject to distortion errors due to RON flatness and RON variation across channels.
The plot in Figure 7 shows the switch on resistance of one of the new fault protected switches across the signal range. As well as achieving very low on resistance, the RON flatness and matching between channels is also excellent. The parts have a patented switch driver design that guarantees a constant VGS voltage and delivers flat RON performance across the input voltage range. The trade-off is slightly reduced signal range where optimal performance can be achieved, which can be seen from the shape of the RON plots. There can be significant system benefits because of this RON performance in applications sensitive to RON variation or THD.
The ADG5404F is the new latchup immune, overvoltage fault protected multiplexer. Latchup immune parts and overvoltage protected parts typically have higher on resistance and worse on resistance flatness than standard parts. However, due to the constant VGS scheme used in the ADG5404F design, the RON flatness is actually better even than the ADG1404 (industry leading low on resistance) and ADG5404 (latchup immune, but not overvoltage protected). In many applications such as RTD temperature measurements, the RON flatness is actually more important than the absolute value of on resistance so the fault protected switch provides potential for increased performance in these systems.
The typical fault mode for a low impedance system is for the drain output to go open circuit in the case of a fault.
.png?h=312&&w=400?mw=290&hash=4358EFBEE66DAA8381DC521296F897E7)
Figure 7. Fault protected switch on resistance
High Impedance Systems
Low leakage, low capacitance, low charge injection switches are most commonly used in high impedance systems. Data acquisition systems are typically high impedance due to amplifier loads on the multiplexer output.
• Leakage is the dominant source of error in high impedance circuits. Any leakage currents can lead to significant measurement errors.
• Low capacitance and low charge injection is also critical for faster settling. This allows for maximum data throughput in a data acquisition system.
The leakage performance of the new ADI fault protected switches is excellent. In normal operation the leakage current is in the low nA range which is critical for accurate measurements in many applications.
Critically, the leakage performance is also very good even when one of the input channels is in fault. This means that measurements can continue on other channels until the fault is fixed, thereby reducing system downtime. The overvoltage leakage current for the ADG5248F 8:1 multiplexer is shown in Figure 8.
The typical fault mode for a high impedance system is for the drain output to pull to the supply rail in the case of a fault.
.png?h=293&&w=400?mw=290&hash=7929317EB7C6A9F1317E9C1FC6B42C80)
Figure 8. ADG5248F Overvoltage leakage current vs Temperature
Fault Diagnostics
Most of the new ADI fault protected switches also feature digital fault pins. The FF pin is a general fault flag which indicates that one of the input channels is in fault. The specific fault pin (or SF pin) is a pin that can be used to debug which specific input is in fault.
These pins can be useful for fault diagnostics in a system. The FF pin firstly alerts a user to a fault. The user can then cycle through the digital inputs and the SF pin will identify which particular switch or switches are in fault.
System Benefits
The system benefits of the new portfolio of fault protected switches are captured in Figure 9. The benefits to a system designer are great, both in terms of ensuring optimal analog performance in a precision signal chain, and in terms of system robustness.
The benefits compared to discrete protection components are obvious and have been described in detail already. The proprietary high voltage process and novel switch architecture also gives the new range of ADI fault protected switches a number of advantages over competitor solutions.
• Industry leading RON flatness for precision measurements
• Industry leading fault leakage current to allow for continued operation on other channels not affected by a fault (10x better than competing solutions)
• Parts with secondary fault supplies for precision fault thresholds while still maintaining optimum analog switch performance
• Intelligent fault flags for system fault diagnostics
.png?h=272&&w=500?mw=290&hash=10AE8C4E60BC5ACC226296CC17420305)
Figure 9. ADI Fault Protected Switch - Features and System Benefits
Application Examples
This first application example shown in Figure 10 is a process control signal chain, where a microcontroller is monitoring a number of sensors such as RTD or thermocouple temperature sensors, pressure sensors, humidity sensors, etc. In a process control application, the sensor may be connected at the end of a very long cable in a factory, with the potential for faults along the length of the cable.
The multiplexer in this case is the ADG5249F which is optimised for low capacitance and low leakage. Low leakage is important for these type of small signal sensor measurements.
The switch operates off +/-15V supplies, while the secondary fault supplies are configured for +5V and GND to protect the downstream PGA and ADC.
The main sensor signal passes through the multiplexer to the PGA and ADC while the fault diagnostics are sent directly to the microcontroller to provide an interrupt in the case of a fault. The user can therefore be alerted to a fault condition and can determine which of the sensors is in fault. A technician can then be sent out to debug the fault and if necessary replace the sensor or cable in fault.
Because of the industry leading low fault leakage specification, the other sensors can continue to be monitored even while one of the sensors is down and awaiting replacement. Without such low fault leakage, a fault on one channel could make all of the other channels unusable until the fault was repaired.
.png?h=289&w=700?mw=290&hash=27CCC3681CFFD7385B7CF3644D6F98F6)
Figure 10. Process control application example
The second application example in Figure 11 is a portion of a data acquisition signal chain where the ADG5462F channel protector would add value. In this case there is a PGA with +/-15V supply rails, while the ADC downstream has as input signal range of 0 to 5V.
The channel protector sits between the PGA and ADC. It uses the +/-15V supply rails as its primary supplies to achieve optimum on-resistance, and uses 0V and 5V for its secondary supply rails. The ADG5462F will allow the signal to pass through in normal operation, but will clamp any overvoltage outputs from the PGA to between 0V and 5V to protect the ADC. Therefore, like the previous applications example, the signal of interest is biased in the flat RON region of operation.
.png?h=321&&w=500?mw=290&hash=C5E26B71365FF9B6C2E5D8B278DABC5B)
Figure 11. Data acquisition application example
Portfolio Summary

Table 1. Low on-resistance family of fault protected switches

Table 2. Low capacitance/low charge injection family of fault protected switches
Summary
Replacing traditional discrete protection components with overvoltage protected switches and multiplexers can provide many system benefits in a precision signal chain. As well as saving board space, the performance benefits of replacing discrete components can be significant.
Analog devices has a wide range of overvoltage protected switches and multiplexers. The latest families of fault protected devices are listed in Table 1 and Table 2. They are built on a proprietary high voltage and latchup immune process and provide industry leading performance and features for precision signal chains.
This article was written by Paul O’Sullivan, Applications Engineer, Analog Devices, Inc.