Our customers understand that success comes to those who prepare. Together, Arrow and Gray Analytics are ready to help your organization position itself for the opportunities that are coming. Cybersecurity and CMMC 2.0 do not have to be complicated, and we’re here to help remove complexity and make complying with CMMC 2.0 easy.
What Is CMMC — and Why Does It Matter Now?
CMMC 2.0, or the second version of the Cybersecurity Maturity Model Certification, is a DoD program that applies to the entire Defense Supply Chain, including Defense Industrial Base (DIB) contractors. It is a unifying standard and a new certification model to ensure that DoD contractors properly protect sensitive information.
This certification is critical to ensuring that contractors adopt appropriate tools and practices to negate cyberthreats to the United States and its interests and that they are equipped to handle the challenges of today’s modern cybersecurity risks.
CMMC 2.0 Matters More Than Ever — and We Can Help
CMMC 2.0 relies on self-attestation by firms contracting with the DoD via the SPRS system. For firms interacting with high-risk controlled unclassified information, they add in additional C3PAO and government-led audits to ensure compliance.
This compliance is essential and can have significant financial impacts for those in non-compliance, even if inadvertent. Non-compliance, even by accident, can mean massive fines.
Arrow + Gray Analytics — Protecting Your Organization and Making CMMC Obtainable
When your organization participates in CMMC 2.0, it means you open your business up to the potential of an audit to ensure compliance. Audits can be time-intensive and take your business away from accomplishing its core objectives.
Arrow, in partnership with Gray Analytics, is your audit defense.
Our partnership acts as a firewall that helps protect your organization and keep it ahead of any issues before they occur. In addition to helping firms achieve their CMMC 2.0 goals with certified third-party auditors, Arrow, in partnership with Gray Analytics, is your self-attestation audit defense, helping you if you do face an audit.
In addition to self-attestation support, we also provide customers who fall into the high-risk Level 2 formal audit category with an end-to-end C3PAO-Specific Assessment Readiness Package that is custom-tailored to remove uncertainty throughout the process.
Our benefits include:
- • Reduced uncertainty on readiness for audit. We ask the right questions and assist with your environment’s interpretation of specific controls based on your chosen C3PAO’s interpretation.
- • Reduced duration of audit. By working through the Assessment Readiness Package, we deliver a ready-to-hand-over packet for you to hand to your C3PAO that matches how the C3PAO prefers to receive the information. This customized, tailor-fit package greatly reduces the amount of time the assessment team has to spend up front, allowing for both shortened time in assessment and reduced lead time to begin the assessment.
- • Reduced cost of C3PAO audit. By reducing the duration of the assessment, costs are reduced (sometimes significantly).
- • Arrow is your end-to-end defense solutions source. Arrow and Gray Analytics have come together to offer a cybersecurity solution built for the needs of defense contractors, but our support for Aerospace and Defense doesn’t stop there. Arrow’s A&D division offers a full-range of mil-spec components and services to support the defense industry. The cybersecurity experts at Gray Analytics provide best-practice services across a broad spectrum of cyber scenarios, from policy and procedure creation to penetration testing. For customers to learn more about Gray Analytics, click here.
The Arrow and Gray Analytics Difference
With the power of Arrow and Gray Analytics, organizations can obtain CMMC 2.0 compliance and be prepared for the future of cybersecurity. Arrow and Gray Analytics do this because we:
- • Ask the right questions. No two organizations are alike. We take the time to understand your business, its composition, its needs, and its goals. We work with you to help you achieve your CMMC 2.0 compliance and build a plan that fits your organization.
- • Have the experience and partnerships. With decades of experience in the fields of cybersecurity and cyber defense, Arrow and Gray Analytics are up to the ever-increasing challenges of today’s cybersecurity landscape. We put our knowledge and experience to use for our partners so that obtaining your CMMC compliance is straightforward.
- • Deploy the right tools. Our suite of proprietary tools helps your organization move with agility and velocity, because opportunity comes at any time.
- • Build for the future of CMMC and beyond. We work relentlessly to stay at the forefront of modern cybersecurity threats and regulations. We help position your organization for sustained success, which includes CMMC 2.0 compliance as well as what comes next. We believe in creating lasting partnerships, not one-off engagements. Our reputation is built on it.
Your Solution Is Here and the Time Is Now
Working with us will start you down the path to CMMC 2.0 compliance. Contact us now to start your consultation and move toward CMMC 2.0 compliance.
Prepare for the future of cybersecurity and schedule your CMMC consultation today