Powerful, energy-efficient Qualcomm® Snapdragon™ processors for embedded devices now available through third-party distribution with long-term support and availability.
SAN DIEGO — September 28, 2016 — Qualcomm Incorporated (NASDAQ: QCOM) today announced that its subsidiary Qualcomm Technologies, Inc. is introducing the Snapdragon™ 600E and 410E processors, for embedded applications in many verticals such as digital signage, set-top-boxes, medical imaging, point of sale systems, industrial robotics, and other Internet of Things (IoT) related applications. Qualcomm Technologies has utilized its mobile investment in Snapdragon processors to introduce solutions for product categories beyond smartphones. The Snapdragon 600E and 410E are being made available globally by third party distributors, initially through Arrow Electronics, for a minimum of 10 years from the Snapdragon 600 and Snapdragon 400 (respectively) product families’ first commercial sampling. This is the first time stand-alone Snapdragon processors are available by distributors, making them accessible in a variety of quantities to manufacturers of all sizes for embedded computing and IoT products.
The introduction of the Snapdragon 600E and 410E processors, along with their global availability by distributors, is an important extension of the Snapdragon embedded product portfolio and its ability to address the needs of highly fragmented consumer, enterprise and industrial categories. The Snapdragon embedded portfolio has a tiered offering that includes development boards, commercial-ready modules, as well as the discrete processors for chip on board designs. These embedded processors offer device manufacturers, solution providers, and system integrators tremendous options for speeding commercialization through a variety of off-the-shelf and custom modules, as well as the freedom for a chip on board design for a cost-optimized approach unique to their requirements.
“Snapdragon is a powerful and versatile processor with many potential applications in a wide variety of IoT applications and we can now offer this technology to a much wider range of customers with the additional benefit of long-term support and availability,” said Raj Talluri, senior vice president, product management, Qualcomm Technologies, Inc. “The Snapdragon 600E and 410E bring together some of our best connectivity and compute technologies to meet the needs for a large range of embedded and IoT applications.”
The Snapdragon 600E featuring 1.5GHz quad-core Qualcomm® Krait™ 300 CPU is the ideal processor for building advanced systems with multi-core performance and immersive 3D graphics, thanks to the Qualcomm® Adreno™ 320 GPU and Qualcomm® Hexagon™ DSP. It supports integrated Bluetooth 4.0/LE & 3.x, 802.11 a/b/g/n/ac and GPS for connected applications. It is also highly expandable for a variety of use cases with SATA, SD3.0, DDR memory, eMMC storage, HDMI, LVDS, HSIC, and PCIe interfaces.
The Snapdragon 410E 1.2GHz quad-core processor offers high performance, low power consumption and rich multimedia with a Qualcomm® Adreno™ 306 GPU and Qualcomm® Hexagon™ DSP. It supports Bluetooth 4.1/LE, 802.11 b/g/n and GPS, making it ideal for IoT use cases in smart homes, digital signage, medical equipment, industrial automation, digital media players and smart surveillance.
“The introduction of Snapdragon 600E and 410E offers a broad range of product options,” said David West, senior vice president, Arrow Electronics. “Arrow looks forward to offering Qualcomm Technologies’ Snapdragon processors and complementing them with the full range of parts and engineering services we can offer to help customers through commercialization.”
With its expertise in connectivity and compute, Qualcomm Technologies is well positioned to deliver the technologies needed in IoT, and has already brought Snapdragon embedded solutions to products as diverse as the Fujifilm Sonosite portable iViz ultrasound system and the Open-Q 410 Wearable Camera Reference Design from Intrinsyc targeting first responder use cases. Built from the foundation of the Snapdragon 600 and 410 processors in the Company’s mobile portfolio, Snapdragon 600E and 410E join a family of solutions to support manufacturers from initial concept all the way to commercialization. Customers have the flexibility to start their evaluation and development with the highly accessible DragonBoard™ 410c community development board manufactured by Arrow Electronics, which is compliant with the 96Boards consumer edition open hardware specification. They can then select from off-the-shelf or custom modules, or choose to use the Snapdragon 600E or 410E with a minimum of 10 years extend life support and availability through 2025, in an optimized chip on board design. More information on the Snapdragon for embedded computing portfolio can be found here.
About Qualcomm Incorporated
Qualcomm Incorporated (NASDAQ: QCOM) is a world leader in 3G, 4G and next-generation wireless technologies. Qualcomm Incorporated includes Qualcomm’s licensing business, QTL, and the vast majority of its patent portfolio. Qualcomm Technologies, Inc., a subsidiary of Qualcomm Incorporated, operates, along with its subsidiaries, substantially all of Qualcomm’s engineering, research and development functions, and substantially all of its products and services businesses, including its semiconductor business, QCT. For more than 30 years, Qualcomm ideas and inventions have driven the evolution of digital communications, linking people everywhere more closely to information, entertainment and each other. For more information, visit Qualcomm’s website, OnQ blog, Twitter and Facebook pages.
Qualcomm Contacts:
Pete Lancia, Corporate Communications
Phone: 1-858-845-5959
Email: corpcomm@qualcomm.com
John Sinnott, Investor Relations
Phone: 1-858-658-4813
Email: ir@qualcomm.com
###
Qualcomm, Snapdragon, Adreno, Hexagon and DragonBoard are trademarks of Qualcomm Incorporated, registered in the United States and other countries. Krait is a trademark of Qualcomm Incorporated.
Qualcomm Snapdragon, Qualcomm Krait, Qualcomm Adreno, and Qualcomm Hexagon are products of Qualcomm Technologies, Inc.
Other products or brand names may be trademarks or registered trademarks of their respective owners