Analog vs digital MEMS microphone: Choosing the best MEMS microphone interface

Explore the differences between analog and digital MEMS microphone interfaces — as well as how to choose the right type of microphone output for your design — in this informative and easy-to-follow article from Same Sky's Bruce Rose.

MEMS (Micro-Electro-Mechanical Systems) microphones have expanded opportunities to add advanced communication and monitoring capabilities into a wide variety of devices. The current popularity of home digital assistants and voice-enabled navigation devices are just a couple of examples that promise to kick-start tremendous growth in voice-controlled electronics. As MEMS technology is starting to dominate market share in the microphone space, it is a good time to examine the types of MEMS microphone electrical interfaces available and how to work with them.

What is a MEMS microphone?

MEMS microphones are typically constructed by placing two semiconductor chips into a single package. The first semiconductor chip is a MEMS membrane which converts sound waves into an electrical signal, while the second chip is an amplifier that sometimes contains an analog-to-digital converter (ADC). An analog output signal is made available to the user if the ADC is not included in the MEMS microphone and a digital output signal is present if the ADC is included.

Analog MEMS microphone interfaces

MEMS microphones with analog outputs allow for a straightforward interface to the host circuit, as shown in the figure below. It should be noted that the analog output signal of the microphone is driven by an amplifier internal to the microphone. Therefore, it is already at a reasonable signal level with a fairly low output impedance.

The dc blocking capacitor (C1) is employed so the dc input voltage of the host circuit does not need to be matched to the dc output voltage of the MEMS microphone. The pole frequency created by the combination of C1 and R1 needs to be set low enough such that the desired audio frequency signals are passed to the host circuit with an acceptable level of attenuation [i.e. for minimum audio frequency range of 20 Hz; 1/(2*π*R1*C1) < 20 Hz].

0719 CUI MEMS Microphones inset

Connecting a MEMS microphone with analog output to an external amplifier

Digital MEMS microphone interfaces

The output signals from MEMS microphones with a digital interface are often encoded with pulse density modulation (PDM). With PDM the analog signal voltage is converted into a single bit digital stream containing a corresponding density of logic-high signals. Some of the advantages of PDM include electrical noise immunity, bit error tolerance, and a simple hardware interface.

The figure below shows how a single digital microphone with PDM output can be connected to a host circuit. Connecting the "Select" pin to either Vdd or Gnd in the figure will determine if the data is asserted on the rising or falling edge of the clock signal.

0719 CUI MEMS Microphones inset rev 2

Single digital PDM MEMS microphone connection

The diagram below shows how two microphones can be connected to the host circuit using shared clock and data lines. This configuration is often employed when implementing stereo microphones.

Schematic of two digital PDM microphones connecting using the same clock and data lines

Two digital PDM MEMS microphones can connect using the same clock and data lines

Choosing an analog or digital output for MEMS microphones

The decision to employ MEMS microphones with analog or digital output signals is often dependent upon how the output signal will be used. An analog output signal is convenient if it will be connected to the input of an amplifier for analog processing within the host system. Examples of conventional analog applications are a simple loudspeaker or radio communication system. MEMS microphones with analog outputs also tend to have lower power consumption than those with digital outputs due to the absence of the ADC.

A digital output signal from a MEMS microphone is advantageous when the signal will be applied to digital circuitry, typically a microcontroller or digital signal processor (DSP). The digital output signal can also be beneficial if the conductors between the microphone and the host circuit are in an electrically noisy environment because the digital output signals will exhibit greater electrical noise immunity than would traditional analog signals.

Conclusion

MEMS microphone technology is here to stay, so it is important to understand the various available configurations. When it comes to choosing an analog or digital output, the decision comes down to how the output signal will be used and what type of system it will be implemented in. Thankfully Same Sky offers a variety of MEMS microphones in either analog or digital (PDM) outputs to help match the specific requirements of your design.

Shop Same Sky's microphones


See related product

CMM-2718AT-42316-TR

Same Sky (formerly CUI Devices) 麦克风 View

See related product

CMM-2718AT-42308-TR

Same Sky (formerly CUI Devices) 麦克风 View

See related product

CMM-3729AB-38116-TR

Same Sky (formerly CUI Devices) 麦克风 View

See related product

CMM-4030DB-26354-TR

Same Sky (formerly CUI Devices) 麦克风 View

Related news articles

Latest News

Sorry, your filter selection returned no results.

We've updated our privacy policy. Please take a moment to review these changes. By clicking I Agree to Arrow Electronics Terms Of Use  and have read and understand the Privacy Policy and Cookie Policy.

Our website places cookies on your device to improve your experience and to improve our site. Read more about the cookies we use and how to disable them here. Cookies and tracking technologies may be used for marketing purposes.
By clicking “Accept”, you are consenting to placement of cookies on your device and to our use of tracking technologies. Click “Read More” below for more information and instructions on how to disable cookies and tracking technologies. While acceptance of cookies and tracking technologies is voluntary, disabling them may result in the website not working properly, and certain advertisements may be less relevant to you.
We respect your privacy. Read our privacy policy here