Motor Driver
Etiquetas similares
High-performance microcontrollers improve the efficiency of motor drives
Motors are widely used in various industrial and consumer products, and are quite common and important electronic components. In addition, with the rapid development of electric vehicles (EVs), the market demand for motors is rising rapidly. How to improve the operating efficiency of motors has become a key element of related applications. This paper will introduce the types and selection factors of motors, as well as the functional characteristics of high-performance mixed-signal microcontroller units (MCU) introduced by ST (STMicroelectronics) which can be used for motor control.
How Wolfspeed power modules are revolutionizing 3-phase industrial low voltage motor drives
Based on the most conservative estimates, electric motors account for more than 50% of all industrial electricity used globally, and 45% of all global electricity. Making industrial motor drive systems even a fraction more efficient would significantly impact global energy consumption and reduce environmental impact. Increasingly stringent efficiency standards are emerging to address energy consumption on a global scale, posing new challenges to power electronic designers.
En la actualidad, C&K forma parte de <br>Littelfuse Inc.
En la actualidad, C&K forma parte de Littelfuse Inc, diseñador y fabricante líder de conmutadores electromecánicos de alto rendimiento y soluciones de interconexión. Su fuerte presencia global abarca una amplia gama de mercados finales, como el industrial, el de transporte, el aeroespacial y el de comunicación de datos.
Los módulos de carburo de silicio desbloquean una mayor densidad de potencia en los accionamientos de motor
This paper presents the CRD600DA12E-XM3 three-phase dual inverter reference design and reveals how its components, including the CAB450M12XM3 power module and CGD12HBXMP gate driver, along with other key technologies, come together in a solution designed to enable next-generation EV traction.