Littelfuse LFUSCD Series Schottky Diodes

Already one of the most trusted names in silicon power components, Littelfuse is at the head of the pack for power conversion solutions with its SiC Schottky diode technology.

As purely silicon-based power components reach their theoretical limits, many industrial companies are looking for new technologies that can meet today’s demands for higher performance. Current industrial power conversion standards require increased efficiency, power density, higher power handling capacity, and a wider operating temperature range. Enter the MPS (merged-PN Schottky) technology, a Silicon Carbide (SiC) diode structure poised to revolutionize the silicon semiconductor industry with its superior electrical, mechanical, and thermal benefits. With global electric power consumption trending consistently upwards each decade, dramatic increases in power efficiency represent a significant opportunity. Developed with efficiency in mind, SiC power devices are expected to reduce electrical energy losses in the power industry by a factor of 100.

Thanks to its near-zero reverse recovery capabilities, the MPS SiC Schottky diode dramatically increases system efficiency and robustness. These enhancements have been realized in industrial power supply, solar, EV/HEV, industrial drives, and welding and plasma cutting markets where its ability to handle high-frequency power switching with negligible losses, enhanced surge capability and extremely low leakage – along with its reduced thermal management requirements – differentiate customers’ solutions from the mainstream.

Technology Breakdown

Silicon carbide’s wide band gap allows superior performance characteristics in comparison to conventional silicon. For a similar breakdown voltage, power devices based on SiC have far lower switching losses by virtue of near-zero reverse recovery, as well as a higher maximum junction temperature. These characteristics equate to high-efficiency power conversion with a substantially reduced need for cooling, which has resulted in smaller, lighter systems.

 

SOURCE: LITTELFUSE

The benefits of Littelfuse’s development efforts are clear. The new LFUSCD Series of SiC Schottky Diodes improves performance appreciably:

Suitable for high-frequency power switching; negligible switching losses; reduced stress on the opposing switch
Larger design margin and relaxed thermal management requirements
Enhanced surge capability and extremely low leakage

Littelfuse Takes the Lead in SiC

 

With a legacy of innovation, proven technical expertise, and the industry’s broadest and deepest portfolio of circuit protection products, Littelfuse has provided objective, comprehensive electrical energy solutions for over 90 years.

Already one of the most trusted names in silicon power components, Littelfuse is once again at the head of the pack for power conversion solutions with its SiC Schottky diode technology. Littelfuse’s SiC power semiconductors dramatically improve application performance, making devices more compact, lighter, and more efficient. Offered in voltage classes of 650 V or 1200 V with current ratings from 4 A to 30 A and two-lead (TO-220) or three-lead (TO-247) packages, Littelfuse’s LFUSCD Series Silicon Carbide (SiC) Schottky diodes are ideal in the following applications:

Power factor correction (PFC)
Buck or boost stages in DC-DC converters
Free-wheeling diodes in inverter stages (switch-mode power supplies, solar inverters, UPSs, industrial drives)
High-frequency output rectification

The Future of SiC is Right Now

The real beauty of materials engineering lies in its dynamic and restless need for advancement. Reaching the next level is not an end game. Every advance in technology is the spark for the next evolution. For SiC, its material properties and technological maturity situate it as the next disruption in power semiconductors. As existing energy technologies advance, so does the need for high-power, low-loss, fast-switching power devices that reduce system complexity and production cost. SiC meets this demand with its unconstrained dynamic behavior—i.e. its ability to reduce switching loses and filtering efforts independent of the limitations of other components—that reduces cost and size while increasing efficiency. The value SiC adds to your devices is immediately identifiable.

We Aren’t All Aerospace Engineers

While SiC proves its potential to enhance power applications at commanding levels, most of us are mere mortals, working on designs that will enhance our daily lives here on Earth. Littelfuse understands that, and they have taken the lead in making SiC technology more accessible by increasing their SiC offerings and making SiC technology the go-to solution for high-demand energy applications.

To date, the biggest challenge next to making SiC more widely available and affordable has been a lack of overall familiarity in the engineering community. As SiC makes its way into server power supplies, power conditioners, solar panels, battery charging systems, and inverters, power device designers will not be long for seeing the enormous potential of the technology. 

Artículos informativos relacionados

Últimas noticias

Lo sentimos, pero su selección de filtros no devolvió resultados.

Hemos actualizado nuestra política de privacidad. Por favor tome un momento para revisar estos cambios. Al hacer clic en Acepto, usted está de acuerdo con la Politica de Privacidad de Arrow Electronics y sus condiciones de uso.

Nuestro sitio Web coloca cookies en su dispositivo para mejorar su experiencia y nuestro sitio. Lea más sobre las cookies que utilizamos y cómo desactivarlas aquió. Es posible que se utilicen las cookies y tecnologías de seguimiento con fines de marketing.
Al hacer clic en "Aceptar", usted está consintiendo la colocación de cookies en su dispositivo y el uso de tecnologías de seguimiento. Haga clic en "Leer más" a continuación para obtener más información e instrucciones sobre cómo desactivar las cookies y tecnologías de seguimiento. Si bien la aceptación de cookies y tecnologías de seguimiento es voluntaria, la desactivación de estos puede resultar en que el sitio web no funcione correctamente, y es posible que ciertos anuncios sean menos relevantes para usted.
Respetamos su privacidad. Lea nuestra política de privacidad aquió