Advanced intelligent autonomous vehicle application technologies and solutions
With the rapid development of IoT, artificial intelligence (AI), and edge computing, intelligent autonomous vehicles have long moved beyond the early stages of simple "toys" and have evolved into highly integrated intelligent carriers. We are witnessing a technological revolution shifting from "machine vision" to "machine decision-making" - advanced intelligent autonomous vehicle application technologies are no longer just about driving more stably or seeing farther. Instead, through deep learning, real-time cloud collaboration, and multi-sensor fusion, they digitize the physical world into actionable and predictable data streams. This article introduces the application types and requirements of intelligent autonomous vehicles, as well as related solutions from onsemi.
Efficient and innovative intelligent autonomous vehicle solutions transforming multiple industries
Thanks to their versatility and innovative efficiency, intelligent autonomous vehicles have revolutionized numerous industries and become indispensable tools across many sectors. In agriculture, intelligent autonomous vehicles assist with precision farming, crop monitoring, and irrigation management, thereby optimizing farm operations and increasing yields. In industrial sectors, particularly construction, mining, and energy, intelligent autonomous vehicles are used for site surveying, infrastructure inspection, and project monitoring.
Intelligent autonomous vehicles are also reshaping delivery services, especially for transporting parcels, medical supplies, and emergency aid in remote or disaster-affected areas. Additionally, intelligent autonomous vehicles are applied in environmental monitoring, public safety, filmmaking, telecommunications, and scientific research. They also play a vital role in security and surveillance, monitoring borders, traffic, and facilities, significantly improving efficiency across various fields.
Intelligent autonomous vehicles contribute significantly to environmental protection by supporting wildlife tracking, forest fire prevention, and pollution control. Emergency services use intelligent autonomous vehicles for search and rescue, firefighting, and disaster response, enhancing public safety and efficiency. The importance of delivery and cargo intelligent autonomous vehicles extends far beyond transportation. They play a critical role in improving supply chain efficiency, reducing operational costs, and minimizing environmental impact. Leveraging advanced technologies, these intelligent autonomous vehicles can accomplish tasks previously deemed impossible or impractical.
Intelligent autonomous vehicles also occupy a crucial role in the media industry, providing photography services for real estate, filmmaking, and event coverage. In telecommunications, intelligent autonomous vehicles assist with network inspections and extending connectivity to remote areas. In summary, intelligent autonomous vehicles have transformed how various industries operate, offering innovative solutions to improve efficiency and safety.
Intelligent autonomous vehicles have evolved from simple remote-controlled devices into sophisticated machines equipped with advanced sensors, GPS, and autonomous navigation systems. This evolution enables them to perform a wide range of tasks, from package delivery to surveillance and inspection. Modern intelligent autonomous vehicles feature high-resolution cameras, depth sensing systems, and artificial intelligence, allowing them to navigate complex environments and make real-time decisions.
The integration of machine learning algorithms has further enhanced intelligent autonomous vehicle capabilities, enabling optimized moving paths, obstacle avoidance, and adaptation to changing conditions. This technological progress has made intelligent autonomous vehicles more reliable and efficient, paving the way for their widespread adoption in logistics. As a result, intelligent autonomous vehicles are now capable of handling diverse applications, from last-mile delivery to large-scale cargo transport.
The integration of artificial intelligence and machine learning enables intelligent autonomous vehicles to autonomously perform complex tasks such as obstacle avoidance, real-time data analysis, and advanced navigation. This advancement not only improves operational efficiency but also expands the range of applications. Furthermore, when integrated with advanced data analytics platforms, intelligent autonomous vehicles empower industries to extract valuable insights from their data, especially in fields like agriculture, mining, and infrastructure.
Cameras and sensors meeting diverse intelligent autonomous vehicle application requirements
Intelligent autonomous vehicle applications are highly diverse. For example, surveying and mapping intelligent autonomous vehicles are equipped with high-resolution cameras and depth sensors to create detailed maps and 3D models for construction, mining, and environmental monitoring. Inspection intelligent autonomous vehicles are used to examine infrastructure such as bridges and pipelines, providing real-time data and detecting issues like cracks and corrosion using thermal cameras and sensors. Agricultural intelligent autonomous vehicles utilize multispectral sensors to monitor crop health, manage irrigation, and apply pesticides or fertilizers, thereby enhancing precision farming.
Delivery intelligent autonomous vehicles are specifically designed for transporting goods and are widely used in logistics, healthcare, and e-commerce for fast and efficient deliveries. Surveillance and security intelligent autonomous vehicles come with high-definition cameras and thermal imaging equipment to monitor large areas and enhance security by detecting intrusions. Heavy-lift intelligent autonomous vehicles are capable of carrying substantial payloads and are used in construction, disaster response, and logistics to transport materials and equipment.
Environmental monitoring intelligent autonomous vehicles are used to assess air and water quality as well as wildlife populations, providing data for research and conservation efforts. Emergency response intelligent autonomous vehicles are deployed in critical situations to deliver medical supplies, locate survivors, and assess damage, enhancing rescue operations with thermal cameras and loudspeakers. Construction intelligent autonomous vehicles can survey sites, monitor progress, and conduct safety inspections, delivering real-time data and high-resolution images for improved project management.
To achieve autonomous intelligent autonomous vehicle navigation systems, image sensors and depth sensors are indispensable components, providing the essential data needed for environmental perception and interaction. Image sensors, such as high-resolution cameras, facilitate visual navigation by detecting and tracking visual landmarks, which is especially beneficial in GPS-denied environments. These sensors enable intelligent autonomous vehicles to identify obstacles, follow designated paths, and make real-time navigational adjustments based on visual input.
The visual data captured by these sensors is processed using advanced computer vision algorithms, allowing intelligent autonomous vehicles to interpret complex scenes and make informed decisions. Depth sensors, on the other hand, generate precise 3D maps of the surroundings by emitting laser pulses and measuring the reflected signals. This technology allows intelligent autonomous vehicles to navigate complex terrains and avoid obstacles with high accuracy, even in low-light or visually cluttered environments. By integrating data from both image sensors and depth sensors through advanced sensor fusion techniques, intelligent autonomous vehicles enhance their situational awareness, enabling sophisticated functions such as obstacle avoidance, precise navigation, and autonomous decision-making.
Global shutter image sensors for intelligent autonomous vehicle sensing systems
When selecting image sensors for intelligent autonomous vehicles, it is essential to consider the specific conditions and requirements of your application. Typically, a system may use six to eight sensors, but configurations with up to twelve sensors are not uncommon. Global shutter sensors capture the entire image simultaneously, making them ideal for moving objects as they prevent image distortion and motion artifacts. This is particularly important for applications demanding high precision, such as mapping, surveying, and industrial inspections. By capturing the entire frame at once, global shutters avoid distortions like the "jello effect" and motion blur, which are common with rolling shutters.
Low-power image sensors offer the advantages of low energy consumption and the ability to be placed in multiple locations, providing a comprehensive view of the scene. Furthermore, High Dynamic Range (HDR) cameras are critical in intelligent autonomous vehicle technology for capturing detailed and accurate images under varying lighting conditions. HDR cameras balance exposure between bright and dark areas, ensuring no detail is lost in challenging lighting environments.
On the other hand, high-resolution sensors like the Hyperlux AR2020, with its 20-megapixel capability, further enhance these features, enabling more detailed and precise inspections and surveys. Additionally, Short-Wave Infrared (SWIR) image sensors can extend vision beyond the visible spectrum.
Image sensor with the lowest power consumption among comparable industry offerings
The AR2020 belongs to onsemi's Hyperlux LP product family. It is a 1/1.8‑inch Back-Side Illuminated (BSI) stacked CMOS digital image sensor with an active pixel array of 5120 x 3840. This advanced sensor captures images in either linear or enhanced Dynamic Range (eDR) modes, featuring a rolling shutter readout. The AR2020 is architected and designed to deliver high-quality performance while consuming very low power. Supported by onsemi's 1.4 µm BSI pixel technology, it provides excellent performance in low-light and NIR wavelengths. The AR2020 offers a powerful edge data capture device that can be programmed through multiple options to deliver optimal bandwidth at extremely low power.
The AR2020 boasts the lowest power consumption among similar products in the industry. It supports enhanced NIR response at 850nm and 940nm wavelengths, as well as Smart ROI (Region of Interest) and Wake on Motion (WOM) functions. It provides multiple subsampling modes including Binning, Summing, Skipping, and Windowing, along with various functional modes such as Global Reset Release (GRR), Trigger, and Context Switching. It also supports enhanced Dynamic Range (eDR) and Line Interleaved HDR (LI-HDR) modes.
The AR2020 image sensor has a wide range of applications, including video conferencing, virtual and augmented reality, machine vision, biometrics, and retail analytics. Common end products include VC endpoints, webcams, video doorbells, AR/VR/XR headsets, machine vision cameras, retail in-store cameras, facial recognition systems, and bodycams.
Meanwhile, Short-Wave Infrared (SWIR) technology can be used to extend vision for intelligent autonomous vehicle navigation systems. SWIR sensors typically operate in the electromagnetic spectrum between 900 nm and 1700 nm. However, some advanced sensors, often referred to as extended SWIR (eSWIR), can achieve wavelengths up to 2500 nm. SWIR photons interact with materials in a manner similar to visible and Near-Infrared (NIR) light, being either reflected or absorbed depending on the material's properties. This makes SWIR sensors particularly suitable for high-resolution imaging under challenging conditions, such as industrial inspection, quality control, and environmental monitoring.
onsemi's SWIR technology, which leverages Colloidal Quantum Dots (CQD) integrated with CMOS sensors, delivers unparalleled imaging capabilities for intelligent autonomous vehicle applications. These advanced SWIR cameras enhance intelligent autonomous vehicle performance in difficult conditions such as fog, darkness, and through obscurants, making them invaluable for industrial inspections, environmental monitoring, and defense surveillance. By providing superior depth perception and 3D imaging capabilities, onsemi's SWIR sensors ensure intelligent autonomous vehicles can collect precise and reliable data, significantly improving operational efficiency and effectiveness across various environments.
For industrial inspections, intelligent autonomous vehicles equipped with SWIR technology can detect material and component defects invisible to the naked eye, ensuring higher quality control. In environmental monitoring, these intelligent autonomous vehicles can assess vegetation health, water quality, and pollution levels with greater accuracy. For defense applications, SWIR technology enhances surveillance capabilities, enabling intelligent autonomous vehicles to operate effectively in low-visibility conditions and detect hidden objects or threats.
Conclusion
Intelligent autonomous vehicle technology has evolved from a simple mobile platform into an intelligent terminal that integrates perception, decision-making, and execution. Advanced application technologies and solutions are reshaping the operational logic of various industries with unprecedented depth, not only reducing human risk and operating costs but also opening up new data-driven dimensions. Looking ahead, with continued breakthroughs in 5G-Advanced, large AI models, and energy systems, intelligent autonomous vehicles will become fully integrated into the digital neural networks of cities and industries. onsemi's image sensors will help manufacturers embrace these advanced technologies and scenario-based solutions, enabling them to maintain air superiority in a rapidly changing competitive landscape and go toward a safer, smarter, and more sustainable future.
Article tags