The importance of multi-turn encoders in industrial automation applications
In industrial automation applications, multi-turn encoders play a key role in ensuring high-precision operation and reliable control of equipment. Compared to single-turn encoders, multi-turn encoders can continuously provide accurate position feedback during long-distance or multi-rotation movements. They are particularly suitable for scenarios such as robotic arms, CNC machine tools, conveyor lines, and automated warehouse systems. This article will introduce the role of multi-turn encoders in industrial automation applications and the features of the solutions offered by Same Sky.
Multi-turn encoders as a core solution for enhancing production efficiency and equipment safety
With the advancement of Industry 4.0 and smart manufacturing, the high resolution and reliable data transmission solutions of multi-turn encoders have become vital for improving production efficiency and equipment safety. By integrating bus communication (such as EtherCAT, PROFINET) and advanced sensing technologies, companies can achieve more flexible control architectures and predictive maintenance, thereby maintaining the stability and advantages of their automation systems in a highly competitive landscape.
A multi-turn encoder is a type of rotary encoder that can track not only the position of the rotating shaft within a single 0° to 360° revolution but also the number of complete rotations. A single-turn encoder repeats its output with every rotation, whereas a multi-turn encoder tracks the full rotations as well as the absolute position within the current rotation.
In many motion systems, knowing the shaft angle within a single 360° rotation is only part of the picture. To accurately track position over time, you often need to know how many times the shaft has turned, especially when that rotation is linked to linear motion, gearing, or larger system movement. This is where multi-turn encoders become essential.
If your encoder only provides a rotation angle from 0° to 360°, you might think, "I'll just track the turns in software." In theory, this approach works: you monitor when the position rolls over from 359° to 0°, or vice versa, and increment or decrement a counter. However, in practice, this method quickly becomes problematic.
This is because missed samples, power glitches, or brief communication losses can lead to incorrect turn count, while noise and vibration can cause distorted position readings, resulting in false turn detection. Furthermore, rapid reversals near the 0°/360° boundary can interfere with the rollover logic and introduce cumulative errors. Most critically, manually tracking turns in software often requires extensive filtering and tuning to achieve accuracy - and even then, it's easy to lose count. Multi-turn absolute encoders solve this problem at the hardware level. They incorporate an internal revolution counter that updates along with the shaft angle, providing a complete position picture without guesswork.
Practical application scenarios requiring multi-turn encoders in industrial automation
In industrial automation applications, situations often arise where single-turn feedback is insufficient, making multi-turn encoders necessary. For example, in gear or belt-reduced drives, if a motor turns 10 times for every output shaft rotation, it's necessary to track those 10 turns, not just the final angle. In ballscrew and leadscrew applications, each rotation translates to a fixed linear distance, so losing track of turns means losing track of position.
Additionally, in rack and pinion systems, the rotary input drives continuous linear travel; knowing the distance moved requires counting the complete shaft rotations. For rotary axes in robotics or automation, such as in rotating platforms, joints, or turrets, understanding cumulative rotation is critical for motion control and collision avoidance. If your system rotates more than 360°, using a multi-turn encoder can reduce software complexity and enhance reliability.
Multi-turn encoders combine two key capabilities: fine angle resolution within a single rotation and a reliable count of full shaft revolutions. Angle sensing is typically handled using technologies like capacitive, magnetic, or optical detection, enabling precise determination of the shaft's position within the 0° to 360° range. To track the number of turns, multi-turn encoders include an internal counter that increments or decrements each time the shaft completes a full rotation. This counter is synchronized with the angle reading to deliver an absolute multi-turn position value.
To address the power-on reset challenge for multi-turn encoders, common strategies include using a Home or Limit Switch. Upon power-up, the system moves to a known mechanical reference point and resets the position from there. Alternatively, storing the last known value can be used. If the system includes a host controller or external memory, it can save the last known angle and turn count. After restart, the position can be reapplied as long as the shaft hasn't moved.
Locking the shaft at startup is another method. For planned shutdowns or ultra-low power standby modes, the shaft can be physically locked in place, and the saved encoder value reloaded on startup. Since the encoder angle and turn count match the previously stored values, the position is restored without movement or error. This approach is especially useful in battery-powered systems or installations where motion is disabled during idle states.
On the other hand, designing for an acceptable loss of turns is also an option. In some cases, absolute multi-turn position across power cycles is not critical. If the system can safely reinitialize at startup or recalibrate based on external sensors, it might be tolerable to undergo a reset process.
Capacitive AMT encoders are ideal for low-power applications
Taking Same Sky's capacitive AMT encoders as an example, they typically consume only about 80 mW, making them very suitable for low-power applications. In comparison, magnetic encoders usually draw between 150 mW and 500 mW, while optical encoders often consume from 200 mW to over 1 W. Capacitive encoders are attractive option in embedded, battery-operated, or power-conscious systems where every milliwatt is crucial.
Multi-turn encoders often provide interfaces such as SPI and RS-485. Although the specific communication protocols vary, most allow easy reading of the angular position and turn count using a small number of bytes or commands. The commands for Same Sky AMT encoders are documented in their respective datasheets. Same Sky also provides sample code tutorials demonstrating how to access the multi-turn functionality from an Arduino. While the integration process is quite straightforward, designing the system around the encoder's startup behavior is vital.
If your application requires position tracking beyond one rotation, involves converting rotary motion to linear travel, uses high gear ratios, needs absolute position with minimal software filtering, or would benefit from simpler, more robust startup logic, then a multi-turn encoder can offer significant advantages.
Same Sky's AMT absolute encoders include compact multi-turn options equipped with SPI and RS-485 interfaces. Designed for embedded systems, they feature low power draw, modular mounting, and simple digital communication, making them ideal for motion systems that require absolute tracking across multiple turns (just remember to manage power-up resets correctly).
If your application cannot tolerate losing the revolution counter during a power cycle, battery backup is one of the most reliable solutions. This method does not rely on recalibration or external sensors but simply keeps the encoder powered during short or extended system power loss. Since Same Sky's AMT encoders consume only about 80 mW, they are exceptionally well-suited for battery-backed operation.
Key takeaways for selecting multi-turn encoders
Multi-turn encoders provide absolute position feedback across multiple shaft rotations, unlike single-turn encoders that reset every 360°. Tracking turns in software is prone to errors due to missed samples, power glitches, and noise; hardware-based multi-turn encoders solve this reliably. Furthermore, applications that demand multi-turn encoders include gear-reduced drives, ballscrews, rack and pinion systems, and rotary axes in automation or robotics.
Effective startup solutions for retaining position include homing switches, saved position recall, shaft locking, or designing for safe reinitialization. Multi-turn encoders may use mechanical, magnetic, or digital methods to count complete rotations. Digital turn counting requires strategies to maintain state across power loss, such as battery backup or startup recalibration. When the persistence of the turn count is critical during power interruptions, battery backup is a reliable option. Capacitive multi-turn encoders, like Same Sky's AMT series, feature ultra-low power consumption (approx. 80 mW), making them ideal for embedded and battery-powered designs. Choose a multi-turn encoder when your system needs to track motion beyond one revolution, convert rotary to linear motion, or could benefit from simplified, robust position control.
Same Sky's absolute AMT modular encoders utilize capacitive sensing technology, offering a highly ruggedized solution without sacrificing accuracy. AMT absolute encoders support 12-bit or 14-bit resolutions and shaft sizes from 2 mm to 5/8 inch, providing engineers with greater flexibility during prototyping without the need to procure additional units, and allowing purchasing managers to significantly reduce the SKU count in production.
The Same Sky AMT absolute modular encoder product line is quite diverse, meeting various industrial application needs. Product series with multi-turn include AMT21, AMT22, AMT24, and AMT25. Please visit the following URL to view all AMT capacitive encoders offered by Same Sky: https://www.arrow.com/en/products/search?q=amt%20encoders&r=true.
Article tags