CGM reference design based on a Silicon Labs BG27 Bluetooth LE chip
Recent advances in microelectronics technology have led to a burgeoning array of wearable medical devices. Things like blood pressure monitors, ECG monitors, and heart rate trackers have revolutionized how we keep tabs on our health. As the underlying components in wearables continue to get more powerful, it becomes possible to use them in more in-depth applications like blood glucose monitoring. This article explores how the new Silicon Labs BG27 Bluetooth LE SoC can be a powerful component in wearable continuous glucose monitors (CGMs).
Introduction
Patients with type 1 or type 2 diabetes must monitor their blood glucose to make informed decisions about their health. Continuous Glucose Monitors (CGMs) allow patients to see how different foods, medicines, or even physical activity can impact blood sugar. This information is crucial to help patients and their medical teams create a data-informed plan of care to prevent possible complications, such as heart attacks, blindness, stroke, or kidney disease.
Candidates for CGMs are those who would like more control in managing their diabetes or those with comorbid conditions that require more engagement with a treatment plan. Patients with type 1 or type 2 diabetes who use CGMs have reported improvements in A1C levels, reductions to hypoglycemia, higher levels of satisfaction in treatment, and a greater level of well-being overall. Advancements in CGM technology even allow for direct communication and coordination with insulin patch delivery systems, acting as an artificial pancreas to continuously monitor and stabilize blood sugar levels.
The Internet of Things (IoT) has changed the way that patients can interact with monitoring their health, and device makers, such as Silicon Labs, are revolutionizing tools that are functional, portable, and energy-efficient for patients. Silicon Labs is proud to share its latest work on its CGM Reference Design.
CGM Reference Design overview
There are several types of continuous glucose monitors, but all CGMs include four main components. These four components include:
Sensor
Analog front end (AFE)
Application processor/Bluetooth receiver
Battery
The sensor is the small wire catheter that is inserted under the skin on the arm or the abdomen and measures the concentration of the glucose level in the fluid between one’s blood. Depending on the type of sensor that someone has, it will need to be replaced periodically; typically, it’s every few weeks.
The transmitter attaches to the sensor and transmits the information the sensor collected to the handheld receiver and/or smartphone that displays glucose concentration data for the patient. Patients can then use this information to evaluate possible changes in glucose levels after eating meals, for instance, or to develop a treatment plan. Silicon Labs has an in-house application that allows patients to see real-time data visualization regarding their results from a CGM.
Wireless devices have opened a wide variety of possibilities for patients to receive crucial information and monitor their health. Device makers have realized the importance of creating products that can incorporate the critical features listed above that are needed for an effective CGM into a portable device for patients. Some of these necessary features include factors like long battery life, energy efficiency, security, and power consumption.
The form factor, or housing, and wireless connectivity are features that are especially important for caretakers, clinicians, and patients. These features allow for continuous, real-time monitoring without a patient needing to be connected via wires to a machine and are a lightweight design so patients can be on the move without concern; CGMs can be worn in the shower or pool, worn while sleeping, and can be worn in most situations. One such device is the BG27 Bluetooth LE SoC from Silicon Labs, which was created with the intention of helping medical device manufacturers incorporate advanced Bluetooth LE connectivity into compact and intricate design devices, such as battery support for medical applications for CGM devices, thus providing the MCU with the ability to run this application as well as its ability to handle power management and store data. The CGM reference design uses the Analog Devices analog front-end (AFE) system.
Silicon Labs is continuing to build upon the successful features that the BG27 brings to the CGM market, and a new CGM based on the BG27 CSP, which will be referred to in this paper as the CGM Reference Design, is currently in development. The CGM Reference Design provides a demo, which includes a simple CGM application based on Bluetooth-standardized CGM profiles and services that pair with a phone. Periodically and at a configurable rate, it reports a value based on the input into the AFE. However, there is not currently a true sensor to take blood measurements, and there isn’t an algorithm to process this data for an accurate blood glucose reading, which is a unique functionality that CGM manufacturers bring to patients.
Highlights of the CGM Reference Design
The CGM Reference Design, currently in production at Silicon Labs, has numerous benefits and improvements for enhanced patient experience, which are outlined in detail below:
Novel Wake-Up Feature: One of the challenges that patients face with CGMs is that the electrical connections for the devices are generally hermetically sealed. Typically, battery-operated devices have a plastic tab to prevent discharge until activation. However, CGM are generally hermetically sealed so this technique can’t be used. A new mechanism on Silicon Labs’ CGM features a way to simulate wake-up for the device with a boost-enable pin when needed. This novel boost-enable pin feature allows the device to work in an extremely low, power-shelf mode until it is woken up by the patient. While this product is in this “shelf mode,” it draws less than 20 nanoamps of current, allowing it to save battery time until the customer uses the new device. This feature means that someone can go into the factory, handle the device in the box, and not worry about draining the battery. Notably, this CGM Reference Design has a novel way of activating this pin. Its activation is triggered by a light sensor, which wakes up the device when it is taken out of the packaging. For instance, a patient can simply shine a phone flashlight at it to make the product active.
Form Factor and Miniaturization of Design: The size of this design was a critical consideration for patients. The battery takes up a significant amount of room on the product, so a small battery is important for the product to be comfortable to wear. The current reference design passes the 14-day market standard and uses the 1.5-volt silver oxide battery, which is also still operational after the 14-day market standard. The goal for the product is to continue to push the limits for the size, as there is still unpopulated space on the device to work with, as well as to capitalize on the length of time it can be worn, with the goal of it being able to be worn for up to 20 or 30 days. For the CGM Reference Design, Silicon Labs decided to provide a baseline implementation that can be further optimized to reduce the overall board space and shrink from the form factor.
Improved Battery Life: The industry is still working to improve battery life and prevent infection at the insertion point. A leading battery provider is currently making a battery to serve as an alternative to the silver oxide battery, which is a lithium-based technology that can handle more electrical capacity and manage spikes that the silver oxide battery can’t currently handle. Currently, the product uses the SR66 button cell battery, but developers would like to eventually use the 716 as it is thinner.
Low Power Consumption: The CGM Reference Design uses a 1.8-volt analog frontend (AFE), which eliminates the use of an external power boost, and because the boost is already inside the chip scale package, it reduces the bill of materials (BOM) count, end cost, and size.
The CGM Reference Design includes applications that take advantage of Bluetooth services and applications that reduce power consumption, too. The user can choose regular updates anywhere between every minute and up to every 30 minutes depending on preference, as far as data reporting is concerned, and the interval of time can be optimized to increase battery life. Silicon Labs has different power modes that allow any Bluetooth device to quickly transition between states to minimize overall power consumption, ranging from optimizing battery power for battery-powered devices to robust solutions for high-performance, long-range needs.
Full Sample Application: During the testing phase for this CGM, Silicon Labs targeted the Bluetooth profiles and services that are necessary for efficient data exchange specific to diabetes management and focused on optimizing this information for increased efficiency and reduced power consumption.
Security Considerations for Data Storage and Privacy: Developers are implementing effective security measures that are necessary for interconnected medical devices in the development of the CGM Reference Design. A large consideration for effective security involves the DTSec protection profile, which is backed by the Diabetes and Technology Society and created in conjunction with the U.S. Food and Drug Administration (FDA). This group looks at the security requirements surrounding life-critical diabetes management devices, including features such as the ability to lock the device, lock the ports, tamper prevention features, and firmware upgrade features to prevent security vulnerabilities. Silicon Labs has included the necessary DTSec Protection Profile requirements for the product’s development. Additionally, Silicon Labs’ Custom Part Manufacturing Services (CPMS) services allow for secure provisioning and device customization, such as bootloader, security key programming, and locking debug during manufacturing, for instance.
Silicon Labs is in discussion about establishing other essential security features for the CGM Reference Design. Now it’s done and should be able to store CGM and temperature data for 30 days, with 1 minute interval. Such data is stored encrypted, so if someone retrieves your CGM can’t use it. Some manufacturers require additional Flash and RAM for data storage, which could be addressed by using an alternative device in the Silicon Labs portfolio.
With the possibility of the device being worn for up to 30 days depending on the frequency of reporting data, there is also an opportunity for patients to use CGMs in the sports and fitness market to monitor biometrics beyond the specifics that someone who presents with type 1 or type 2 diabetes might require. Other benefits include improving sleep and optimizing food intake.
Moving forward
Developers are continuing to optimize this CGM reference design for the consumer so that they can feel confident in monitoring their health with the latest tools and technology. Silicon Labs continues to expand its portfolio of solutions to address various needs as technology evolves. It will continue to work closely with leaders in the industry to grow its portfolio as major players in the CGM and portable medical device market rely on Silicon Labs for expertise. The team is actively strategizing ways to ensure that patients receive a product that not only exceeds expectations but is also secure and efficient. Silicon Labs is available for support regarding the reference -time-” should be the reference design.
Article tags