Types and selection tips for DIP switches
DIP (Dual Inline Package) switches are common electronic components often used in digital circuits to configure or set different functions. Due to their ease of use and reliability, DIP switches have found widespread use in many applications. This article will introduce the types and characteristics of DIP switches, as well as the DIP switch solutions offered by Same Sky.
DIP switches facilitate the configuration of electronic product functionalities
DIP switches have been a staple in electromechanical devices since the 1970s, allowing users to manually alter electronic circuits. Their simplicity, flexibility, and low cost have ensured their long-term use in a variety of electronic applications. They come in various sizes, configurations, switching mechanisms, and power ratings. Customers can choose the number of positions on DIP switches based on the configuration options required for their application. Some DIP switches can be toggled manually, while others may require special tools or screwdrivers to toggle the switch positions.
The operation of DIP switches is based on mechanical contacts. Each switch contains one or more mechanical contact that either connect or disconnect circuits at different positions. The construction of the switch allows it to toggle between different positions, altering the connectivity status of the circuit. When the switch is in one position, the corresponding circuit is connected, while it is disconnected in another position.
A DIP switch is a dual in-line package switch, meaning it consists of a series of switches within a single unit. It is an electromechanical device that requires users to manually move actuators to activate or deactivate different electronic circuits. DIP switches are typically mounted on a PCB or breadboard, allowing users to quickly preconfigure or switch between various settings or operational modes of electronic devices.
The principle and operation mode of DIP switches
The principle of any switch involves understanding the concepts of poles and throws. DIP switches can be categorized into single-pole, single-throw (SPST), single-pole, double-throw (SPDT), and double-pole, double-throw (DPDT) switches. Each SPST switch in a DIP switch can only control the circuit to be either open or closed, having only one fixed position; each SPDT switch individually controls one circuit and has two fixed positions; each DPDT switch simultaneously controls two circuits and has four fixed positions.
An SPST switch means that the device in an electronic circuit is either closed to allow current flow or open to interrupt current flow. An SPDT switch can select between two different current flow paths. In other words, moving the actuator does not interrupt the current but redirects it into a different circuit branch.
A DPDT switch uses two linked switches to control two circuits simultaneously. When one switch toggles positions, the other switch performs the same action. Each switch redirects the current to different paths within its circuit. Technically, multiple switches can be connected in this arrangement, enabling multi-pole, multi-throw functionality.
The number of switches in a package depends on the application, ranging from 1 to 16 positions or more. Common DIP switch packages include eight positions because it corresponds to 256 possible binary codes, equivalent to one byte of data.
DIP switches are commonly used to set and configure various parameters or functions in digital circuits. For example, they can be used to configure the address of a microcontroller, allowing multiple devices to operate on the same bus. In some applications, DIP switches can be used to select different power sources to provide redundancy or backup power.
DIP switches are frequently employed to switch between different operating modes of a device, which is particularly useful in some control applications, such as adjusting the sensitivity of sensors or switching display modes. DIP switches can also be used to enable or disable specific features of a device, providing greater flexibility in design.
Types and functional characteristics of DIP switches
DIP switches come in various types, including slide actuator, piano actuator, rotary actuator, and more, each with its own application characteristics, allowing for selection based on specific needs.
Slide
The slide DIP switch is a standard toggle switch, with each switch having two positions—closed or open (also labeled as on/off or 1/0)—and can be used as a SPST switch. There are also three-position slide DIP switches, featuring a central neutral position and one contact on each end, typically configured as on/off/on. Any DIP switch can be configured as normally open (NO) or normally closed (NC). Normally open switches complete the circuit upon activation, while normally closed switches break the circuit upon activation.
Slide DIP switches typically consist of a series of sliders, with each slider corresponding to a switch position. By moving the sliders, users can change the corresponding switch states. Slide DIP switches can provide encoding functionality and customizable switch counts. Due to their mechanical structure, slide DIP switches generally offer durability, making them suitable for applications requiring frequent switching.
Piano
The piano DIP switch is similar to the slide DIP switch. However, unlike the slide switch that is horizontally oriented and moved forward and backward to actuate, the piano DIP switch is vertical and requires upward and downward movement, earning its name from its resemblance to piano keyboards. This type of switch is commonly used in applications that require fine adjustments or selections among multiple positions.
Unlike traditional discrete-position switches, the piano DIP switch offers continuous adjustment capability, providing a good human-machine interaction experience. Due to its continuous adjustment feature, piano DIP switches typically have higher resolution, allowing for finer control during adjustment. Some piano DIP switches are designed in the form of adjustable resistors or capacitors, making them suitable for applications that require fine-tuning of circuit characteristics.
Rotary
The rotary DIP switch is a special type of DIP switch characterized by its rotary operation instead of sliding or pressing. This switch is commonly used for configuring electronic devices, allowing users to rotate between different positions to change the circuit's configuration or functionality. As the user rotates the actuator in a circular motion, the rotary DIP switch changes positions, with the amount of rotation determining the switch's output.
A rotary DIP switch with four output pins can produce up to 16 different binary-coded output configurations. It can also be configured to operate as a SPDT switch device, with the single pole possibly having three or four throws. The 16-position rotary DIP switch uses hexadecimal codes of 16 symbols to describe output combinations. The hexadecimal code uses the digits 0 to 9 and then the letters A to F.
Some other types of DIP switches include rocker actuators, which operate similarly to a seesaw. The switching mechanism rocks between two positions, lowering one side of the actuator raises the other, making them just another variant of basic toggle switches.
Key specifications and applications
The manufacturer's datasheet provides basic performance and specification information for each DIP switch, which is crucial for selecting the best DIP switch for a specific application. In addition to obvious specifications such as the number of positions and actuator type, there are some additional specifications to consider. For example, the type of mounting method: surface-mount DIP switches are suitable for PCBs, while through-hole versions are used for breadboards. The terminal style of DIP switches can also be categorized into gull-wing, angled gull-wing, J-hook gull-wing, PC pin, and crimped PC pin, allowing for different mounting options based on requirements.
DIP switches typically support a rated voltage ranging from 2.4 to 50 Vdc, with the maximum voltage specified on the device. The rated voltage usually lists both the switch voltage and non-switch voltage. The switch rated value indicates when the actuator moves from one position to the next. The non-switch rated value is the rated value when the actuator is in a stationary position, typically higher than the switch rated value.
The rated current supported by DIP switches typically ranges from 10 to 200 mA, which represents the maximum current the device can handle. The pitch of DIP switches is usually between 1 to 2.54 mm or 0.039 to 0.1 inches, indicating the center-to-center distance between pins. The IP rating supported by DIP switches is also crucial and can be classified as rated or non-rated, representing the ability to prevent moisture and dust ingress.
Ensuring that the selected DIP switch meets the performance standards of the design is essential. Using DIP switches beyond their specifications may lead to issues such as arcing or self-welding. It can also affect the device's performance or render it inoperable.
For decades, DIP switches have been widely used in various applications, and they have even found new uses in IoT devices. They serve as a quick method for pre-configuration or reprogramming of devices before implementation in smart homes or factories, thereby minimizing downtime. Some of the most common applications of DIP switches include programming garage door openers, remote controls, configuring options on PC expansion cards or motherboards, adding new devices to IoT networks through simple user configuration, and checking the configuration of industrial equipment without the need for powering up the device.
Conclusion
DIP switches were originally introduced as a simple way to alter the characteristics of electronic systems, allowing for configuration changes during manufacturing or by users. Over time, advancements in software switches and user interfaces have reduced their widespread use, but due to their low cost and ease of use, they remain well-suited for a variety of electromechanical devices. By understanding DIP switches and the available variants, these applications can configure devices to perform specific functions and communicate with other matching devices.
Same Sky offers a wide range of DIP switches to meet the needs of different applications, including piano, rotary, and slide actuator types, with pitches of 1.27, 2.54, or 5.08 mm, 1 to 16 positions, and surface mount or through-hole mounting styles. Same Sky's DIP switches feature flat or raised actuator levels, various terminations, and short, long, or SMT pins, making them a flexible choice for industrial, commercial, or telecom applications. Several models of DIP switches from Same Sky also offer IP67 protection ratings. For more information on the specifications of DIP switches, please visit the Same Sky's website. You can also visit Arrow's website directly to make purchases.
Article Tags