Arduino Uno vs. Mega vs. Micro

Published By

The Arduino boards have become one of the most popular microcontrollers on the market with a huge variety of boards. Some Arduino boards are better suited for certain applications. Let’s compare some of the more popular boards that Arduino has created – the Uno, Micro, and Mega 2560 – and see which one is best for your next prototyping, IoT or DIY project, or school robotic project.

Arduino Board Size & Pricing Comparison 

The Micro comes in, being true to its name, at 0.7” x 1.9” making it one of the smallest microcontroller boards out there. On the opposite side of the spectrum, the Arduino Mega 2560 board dimensions are about 4” x 2.1”, making it about 6x bigger than the Micro in terms of area size. Arduino Uno dimensions of 2.7” x 2.1” fall somewhere in between the Micro and the Mega 2560. The pricing for Micro is usually around $19-25 (can be hard to find stock) while the Uno runs around $20-23, and the Mega 2560 comes in at $36 - $39.

Connectivity

To get connected to your computer and start coding, both the Uno and the Mega 2560 can easily connect with a Standard A/B USB cable, while the Micro will need a Micro-USB cable.

Each of these Arduinos have a different number of I/O pins. The board with the most pins is the Mega 2560, which comes in with a whopping 54 Digital I/O pins (were 15 of them have PWM) and has 16 Input Analog pins. Surprisingly, the Micro has the 2nd most pins out of the three, having 20 Digital I/O pins (with 7 of them having PWM) and 12 Input Analog pins. Coming in last is the Uno, which has 14 Digital I/O pins (with 6 of them having PWM) and 6 Input Analog pins.

Also good to note, is that both the Uno and Mega 2560 usually come in as through-hole, while the Micro’s pin layout of its header I/O’s allows it to fit into any breadboard or system. This means that most Shields are compatible with the Uno and Mega 2560, but the Micro will be out of luck.

You can check out some of the more helpful and interesting Arduino Shields, including the 1Sheeld+ (uses your smartphone as sensors) or a Relay Shield:

See related product

Relay Shield | 103030009

Seeed Technology Co.,Ltd Development Kits and Tools View

See related product

1SHEELD+

Integreight, Inc View

See related product

Bluefruit LE Shield | 2746

Adafruit Industries View

See related product

2.8"" TFT Touch Shield | 1947

Adafruit Industries Development Kits and Tools View

Processing Power

All three Arduino boards have their own level of processing power, so let’s talk about their frequency/clock speed. The frequency/clock speed on these boards simply means how fast it can execute commands. It was a nice surprise to see that they all have the same clock speed at 16 MHz.

The Flash memory on the Uno and Micro are the same at 32 kB, while the Mega 2560 has 256 kB, giving it 8x more memory space! The Flash memory simply means how big of a sketch/code you can upload to your Arduino, therefore if you have a hefty code the Mega 2560 is the way to go.

Arduino boards use SRAM (Static Random-Access Memory). The Mega 2560 has the most SRAM space with 8 kB, which is 4x more than the Uno, and 3.2x more than the Micro. With more SRAM space, the Arduino has more space to create and manipulate variables when it runs.

Conclusion

The Arduino comparison table below shows a side-by-side comparison of the Uno, Mega 2560, and Micro.

Arduino Comparison Chart 

Figure 1: Arduino Uno, Mega 2560, and Micro comparison.

 

For a bottom line of which board you should use, it breaks down like this:

Which is the Best Arduino Board for Your Project?

- If you’re worried about the compactness of your project, not too worried about the number of I/O pins, don’t mind spending a bit more than the usual price (it might be hard to find), and don’t want to add any Shields, go with the Arduino Micro.

- If you are writing large code, need a lot of I/O pins for your project, and want it to have a Shield, then the Arduino Mega 2560 will work for you.

- And, if you just want to prototype something small, want to add a Shield, want a cost-effective option, or just want to have fun learning code, the Arduino Uno is for you.

See related product

A000093 | Arduino Micro

Arduino S.r.l. Embedded System Development Boards and Kits View

See related product

A000067 | Arduino Mega 2560 Rev3

Arduino S.r.l. Embedded System Development Boards and Kits View

See related product

A000066 | Arduino Uno Rev3

Arduino S.r.l. Embedded System Development Boards and Kits View

To see more comparisons, check these out:

Comparing PocketBeagle Specs and Raspberry Pi Zero Specs

Raspberry Pi 3 Vs. Raspberry Pi Zero W

Related news articles

Latest News

Sorry, your filter selection returned no results.

We've updated our privacy policy. Please take a moment to review these changes. By clicking I Agree to Arrow Electronics Terms Of Use  and have read and understand the Privacy Policy and Cookie Policy.

Our website places cookies on your device to improve your experience and to improve our site. Read more about the cookies we use and how to disable them here. Cookies and tracking technologies may be used for marketing purposes.
By clicking “Accept”, you are consenting to placement of cookies on your device and to our use of tracking technologies. Click “Read More” below for more information and instructions on how to disable cookies and tracking technologies. While acceptance of cookies and tracking technologies is voluntary, disabling them may result in the website not working properly, and certain advertisements may be less relevant to you.
We respect your privacy. Read our privacy policy here