Skip to main content

RoHS Explained

Latest Updates | Complexities to Consider | Exemptions | Official Documents

RoHS: The European Union (EU) Directive on the Restriction of certain Hazardous Substances. EU Directives must be transposed in each EU state into binding National legislation. This will restrict the use of certain substances in electrical and electronic equipment placed on the EU market beginning July 1, 2006.

The Directive seeks to limit the chance of hazardous substances possibly leaching out and polluting the environment during end-of-life recycling or disposal in landfills. The electronics industry is most affected by the restriction on lead, as it is a key component in electronic component packaging (pins), solders and solder pastes. While the term “lead-free” is sometimes used to describe RoHS, the real requirement for manufacturers is to design and ship products that are not only lead-free but fully RoHS compliant, meaning they do not contain more than the allowances of any of the hazardous substances named in the directive.

The hazardous substances and the proposed maximum concentrations levels are:

lead – Pb

.1% max concentration

mercury – Hg

.1% max concentration

cadmium – Cd

.01% max concentration

hexavalent chromium – Cr(V1)

.1% max concentration

polybrominated biphenyls – PBB

.1% max concentration

polybrominated diphenyl ethers – PBDE

.1% max concentration

 

Read the full text of EU Directive 2002/95/EC on the restriction of the use of certain hazardous substances in electrical and electronic equipment.